Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
AM64x boot ROM supports booting from parallel GPMC-NAND. From "4.4.10 GPMC NAND Boot" in AM64x TRM "AM64x ROM only supports boot from ONFI 1.0 compatible 8 bit parallel NAND memory up to…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: UNIFLASH , AUDIO-AM275-EVM
The ENETFOTA example demonstrates how Ethernet can be used to transfer a new application image from a host PC to an AM275x device that is currently running an older application…
Part Number: MSPM0G3507
mcan_application_LP_MSPM0G3507_nortos_ticlang_20260408.zip
Here is the mcan application demo code for user easily start to used MSPM0 mcan module.
User can choose to use either fifo or buffer Tx/Rx, or combine Tx FIFO and…
Part Number: TPS37100-Q1
Hi,
Currently I'm using discrete approach to monitor the battery rail for overvoltage and undervoltage faults and I'd like to understand is there a single package solution, which can help solution cost and size?
Best Regards…
Part Number: AM13E23019
Hi experts,
Is early brownout detection (with interrupt) possible? How to configure thresholds?
"7.8.1 Power Management Unit (PMU): section in datasheet mentions "Brownout reset (BOR) supply monitor with early warning capability…
Part Number: AM13E23019 Other Parts Discussed in Thread: SYSCONFIG
Hi experts,
I wanted help with the Timer module configuration of the AM13E30x sysconfig. I open the example.syscfg and try to configure the timer, but notice the following issues:…
Part Number: TMS320F280033 Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH
The default boot to flash entry point is 0x80000 in the F28003x Boot ROM, which is not in the memory map for the F280033/F280034 subset parts. This thread will detail how…