Other Parts Discussed in Thread: SN74LVC1G123 FAQ: Logic and Voltage Translation > Output Parameters >> Current FAQ
The answer to all three questions is "yes" - these are the three primary uses of open-drain outputs on logic devices. Much of this also…
Other Parts Discussed in Thread: SYSCONFIG Overview:
SysConfig provides extensive support for working with a board including the ability to remove all board constraints and work at the device package level. However, using this feature may cause unexpected…
Other Parts Discussed in Thread: TMS320F28069 , TMS320F28035 , TMS320F28027 , CONTROLSUITE , DRV8312 What are the resources to implement Trapezoidal Control of BLDC Motors with Hall Effect Sensors using C2000 MCUs?
Best, Matthew
Other Parts Discussed in Thread: SN74LV221A , SN74LVC1G123 , SN74LV123A , SN74221 , SN74LS221 FAQ: Logic and Voltage Translation > Monostable Multivibrators >> Current FAQ
For the majority of MMV devices, y es, the Cext pin can be grounded.
The Cext…
FAQ: Logic and Voltage Translation > Monostable Multivibrators >> Current FAQ
The output pulse width (tw) is determined with the following equation:
tw = K * R * C
with R := external timing resistor, C := external timing capacitor, K := timing constant…
Other Parts Discussed in Thread: TMUX1247 , TMUX1237 Parasitic inductance due to the length of PCB traces can cause overshoot and ringing during switching events. The output voltage may briefly exceed the expected output voltage value, due to overshoot…
Other Parts Discussed in Thread: SN74LV221A FAQ: Logic and Voltage Translation > Monostable Multivibrators >> Current FAQ
Unused channels for a logic monostable multivibrator (MMV) such as the SN74LV221A should be terminated such that:
(1) All inputs…
FAQ: Logic and Voltage Translation > Monostable Multivibrators >> Current FAQ
The above functional block diagram shows generally how a monostable multivibrator (MMV, or one-shot) works. Not all of them have every part shown, but this is the most common…
FAQ: Logic and Voltage Translation > Logic Technology >> Current FAQ
It's very common for people to refer to "TTL logic" and to actually mean "5V logic" -- but how are they different?
The key difference is in the input and output voltages. This graphic…
The public documentation of TISCI user guide is hosted at http://downloads.ti.com/tisci/esd/latest/ . But current documentation hosted in public does not have the J721e specific chapter. Where can I find this information?