Other Parts Discussed in Thread: CC2340R5 Hello,
I am using CC2340R5 board,(simplelink_cc23xx_sdk_6_40_00_21_eng) SDK, Code Compiler studio 12.0.0
Using this controller board since a month, this issue never occurred in the past.
Today while flashing…
Part Number: CC2340R5 Other Parts Discussed in Thread: LP-XDS110ET Tool/software: Hi experts,
We made the board using CC2340R52E0RGER(4*4, 24pin).
however, when connecting LP-XDS110ET with it, an error occurs as shown below.
[ERROR] Cortex_M0P:…
Part Number: CC2340R5
Tool/software:
Hello,
We have made a custom board with CC2340R5. To flash the chip, we have XDS-110ET REV B module. We are using a code composer studio. Below is our pin connection with XDS-110 and custom CC2345 board
…
Other Parts Discussed in Thread: CC2340R5 Hi team,
For CC2340R5 PG1.0, we need to flash a default CCFG file for a blank device. (workaround to resolve the “Error -1274 @ 0x0” flashing error).
For PG2.0, is this fixed ? Customer doesn't need to flash…
I also used to run data stream and many time i get below
Debugging is not allowed. If this is not expected, check your CCFG. If you are experiencing issues with loading your application, do the following (this will erase the chip): - Code Composer Studio…
Hi Simbasoft,
Did you follow the instructions for flashing a blank device from the Quick Start Guide? For CCS:
The procedure detailed below should be followed if flashing a blank device or a device that has been mass-erased. If the procedure is performed…
Hi Ryan,
I followed the steps you provide.
1.Performa a complete chip erase (CHIP_ERASE or otherwise).
2.Flash your CCFG again and check with Uniflash that the area was updated correctly, and save expected flash memory for later comparison.
This…
Part Number: CC2340R5 Tool/software: Hi - I am well along in developing for the CC2340R5 and last week upgraded CCS to version 20.0.0 which of course is all new. I am debugging with two dev boards on one machine and have been running for a very long time…
Other Parts Discussed in Thread: CC2340R5 , SYSCONFIG , UNIFLASH , LP-EM-CC2340R5 Hi,
I have an issue that is similar to the one described by Simbasoft in this previous thread (which was locked by Clément before I could post):
https://e2e.ti.com/support…
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: UNIFLASH , CC2340R5 LP-EM-CC2340R5 with XDS110ET Debugger
Windows 11 Home x64
CCS v12.3.0
Uniflash v8.3.0
simplelink_lowpower_f3_sdk_7_10_00_35 installed
I have looked at these…