Hi Toby,
I had tried by doing reset on the launchpad after running the zigbeeHAgw.BUt then also i am getting SRSP Timeout.
And I am unable to send commands.The SRSP Timeout issue is getting at starting level only.Now the baudrate is set to 921600…
Hi all Thanks very much
I am trying to run the Zigbee Gateway on a Zitara AM4378 with a CC2531USB according to the picture hardware.jpg.
I have followed in the steps of IT Z-Stack - Zigbee Linux Gateway Project Zero. The web application shows the…
Alvin Chen I find if I connect LAUNCHXL-CC26x2R1 to test ZIGBEE-LINUX-SENSOR-TO-CLOUD_1.0.0 on my Ubuntu VM. I always see the following error. Do you see the same problem?
[13:17:33.754,768] [NWK_MGR/MAIN] UNMSKBL: [13:17:33.758,759] [NWK_MGR/MAIN…
Hi YiKai Chen
the zibgee linux gateway seem that it no-normal run on ubuntu1604.
sometimes it can,I want to test the zigbee ota end device.this is the log.
Fullscreen
5670.packet log.txt
Download
starting ZLSZNP, cmd ' ./ZLSZNP_x86…
Complete logs when I run ' zigbeeHAgw ' file.
-------
Startup phase 3 failed waiting for Zstack linux to exit waiting for NPI to exit making sure there are no lingering servers... there are 0 NPI servers there are 0 ZLS servers there are 0 GATEWAY…
Part Number: CC2652P Hello All,
I am using CC2652P & simplink sdk v5.20 based ZNP along for Raspberry pi over UART and zigbee 3.0 linux gateway.
The Gateway has stopped working after being operational for around 1 year.
here is the details/log when…
Hi Ryan,
Please check the error.
log:
Platform type selected automatically as bbb. To override this selection, please stop this script, and then run it again, specifying the desired platform type at the command line: ./zigbeeHAgw [help | bbb …
When i start the "zigbeeHAgw " - It always throws the error as shown below-
pi@raspberrypi:~/Desktop/zigbee_gateway_v3.0/out/Precompiled/servers $ sudo ./zigbeeHAgw
Platform type selected automatically as bbb.
To override this selection, please stop…
Part Number: LP-CC2652RSIP Other Parts Discussed in Thread: UNIFLASH , , CC2652RSIP , LAUNCHXL-CC26X2R1 , CODECOMPOSER , SIMPLELINK-CC13XX-CC26XX-SDK Hi, colleagues!
I faced the issue during ZIGBEE-LINUX-SENSOR-TO-CLOUD evaluating.
I followed all…
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1 , CC2531EMK Tool/software: Linux
I am running into a problem while building Zigbee_3_0_Linux_Gateway_1_0_0 to x86 platform. I have changed target platform in the build script to x86 i.e. in $(INSTALL_DIR…