Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: TDA2
HI TI erperts:
有两个问题帮忙解答 下
1 参照MMWCAS-DSP-EVM设计级联雷达处理板中,能否将DEMO板中的60 pin MIPI JTAG口换成14 pin的JTAG仿真器标准座子? 即去掉EMU信号,如果可以需要哪些注意事项?
2 换成14 pin的JTAG仿真器标准座子, 可能会有哪些影响?比如哪些功能不支持,或者速度变慢等。
Our records show the following:
1) T04973562: The order was rejected; Payment also failed ( 4/14/24 1:32:00.602 AM)
2) T04972689 : The order was rejected; No record of payment made
3) T04974201: The order was rejected; No record of payment made
If you can produce…
Hi Mr. Park,
Thank you for clarifying. Please see below for the configuration file as requested. In addition, should you have more questions or need of assistance to help with DPD tuning and triggering, please don't hesitate to let the team know. We would…
Part Number: SK-AM62A-LP
Hello,
I was trying to implement the edgeai-gst-apps-barcode-reader available here:
https://github.com/TexasInstruments/edgeai-gst-apps-barcode-reader
I was trying to implement using docker. I am getting error messages. How to…
Pin 11 is a digital input; you must not try to apply analog voltages to it. The output is defined only for valid logic levels, i.e., for voltages near 0 V and 3.3 V.
Pin 10 must not be left floating.
This device already handles the RS-232 bus voltages…
Hi,
Just now i found one thing, maybe it is not your code or configuration mistake.
As you can see in above schematic, there was a demux connected to the NHET1[08], NHET1[10] and NHET1[14]. That means these pins are using for multiple functionalities based…
Andreas Dannenberg said: So your status is still exactly the below?
No, we currently see the following error messages.
Leo Yang said: root@am62xx-evm:~# dmesg | grep spi1
[ 5.381390] qcaspi spi1.0: ver=0.2.7-i, clkspeed=8000000, burst_len=5000, pluggable…