Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: 66AK2E05 We are working a potential SGMII issue utilizing one of the TI Keystone processors (66AK2E05) and I want to be able to update the transmitter voltage (we boot from FLASH). Looking at one of the guides, SPRUHO3A, there is a register…
Part Number: 66AK2E05 Other Parts Discussed in Thread: DA8XX Hi ,
We face following kernel panic issue :
Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.4.117 (ide@tmnsrv) (gcc version 8.4.0 (Buildroot 2021…
Part Number: 66AK2E05
Hi!
I want use in my project NAND FLASH with boot from NAND.
If possible, can I use more NAND memory than 4 GB?
Can you recommend specific chips?
__________________________________________________
Can I use 2 x 4GB memory in parallel…
Part Number: 66AK2E05 Hi!
If I am not using the SGMII ports (SGMIIRX2-SGMIIRX7 and SMIITX2-SGMIITX7) in my project, can I leave them unconnected or do they need to be pulled somewhere?
When connecting NAND memory, I do not use the EMIF A0-A10, A13 - A23…
Part Number: 66AK2E05 Other Parts Discussed in Thread: 66AK2H14 Hi, all
Now I have two board to compare the speed.
One board is the custom board which using 66AK2E05.The other is EVMK2H board which should using 66AK2H14
Both boards only run…
Hi,
Sorry for delayed response.
1. Can 66AK2E05 achieve TRUE 10GbE data, we want to be able to reach 10G speeds.
Yes, we can achieve TRUE 10GbE data.
2. Can we reach 10GbE speeds for BOTH ports of the 66AK2E05.
Yes, we can achieve TRUE 10GbE speed in…