Part Number: 66AK2G12 Dear All,
with the latest CCS version 12 I am not able to run a software on my 66AK2G12 C66 core with our Blackhawk Emulators.
Each time I want to load software it is seems to do someting but nothing happens.
For now I stick to CCS…
Other Parts Discussed in Thread: CLOCKTREETOOL Hi, Experts
We are considering how to operate GPMC_CLK=100MHz while keeping the DSP/ARM clock at 1000Mhz using ClockTreeTool. The current design is to input 24MHz to SYSOSC and SYSCLK1=1000MHz with PLL_MAIN…
Other Parts Discussed in Thread: 66AK2G12 Hi,Experts
In page 1202, Table 7-127 of the 66AK2G12 data sheet (spruhy8i) The DDR on the evaluation board has a Row Address of 16bits, but the DDR on the custom board has a Row Address of 15bits.
Can the 66AK2G12…
Part Number: 66AK2G12 We have a successful 600 MHz design that we would like to migrate to 1000 MHz. Is there a comprehensive migration guide?
What are the required changes? Hardware voltages/bootloader PLL initialization, DDR clocks?
Thank you
Hello Jeremy,
Sorry for the delayed response. Unfortunately we do not directly support this device now. But it seems like this device should boot via eMMC. Are you trying to boot via UDA in fs mode?
regards,
Judith
Part Number: 66AK2G12 Other Parts Discussed in Thread: TIDA-01414 , TPA3244 ,
Hi Support Team,
My customer is trying to reference Dolby Atmos® decoding and rendering using the 66AK2G audio SoC as realized in TI's reference design at the following site…
Hi,Paul
I found the following thread which seems to be the same phenomenon. Are these measures effective?
66AK2G12: POR doesn't work e2e.ti.com/.../66ak2g12-por-doesn-t-work
- Last Thread - I think I found the reason why POR does not working. The pin…
Bernhard Seiz said: Or are we going into a totally wrong direction? Is there a simplier approach? Do we need a multi EMAC processor?
It does seem like you are thinking of hacking up Ethernet addressing in quite complex ways, wanting the 66AK2G12/C6657 to…
Part Number: 66AK2G12
Hi Support Team,
My customer will be using 66AK2G12 RTOS_SDK to evaluate with EVM. Checking the following site, CCS is supposed to use the latest version, but the latest version at the time of the SDK release seems to be CCSv7. …