Part Number: 66AK2H06 Hi
I have following queries..
1) How many MACs are there in 66AK2H06 ?
2) Are all are configurable ?
3) Is it possible for any device (connected at port 1) to exchange data with any other device (connected at port 2 / 3 / 4) without…
Part Number: 66AK2H06
Hi,
The customer's board will share 1.8V and 1.5V with other SoC device supplied to the 66AK2H06.
The power-up sequence of 66AK2H06 is CVDD --> CVDD1 --> +1.8V --> +1.5V --> +0.85V. However, in order to counter the…
Part Number: 66AK2H06 Hi all,
I am confused in TI-RTOS and process-SDK RTOS.
66Ak2H06 is a mulicore soc. which DSP core I could run TI-RTOS or processor-SDK RTOS?
or those RTOS must run in arm core?
Regards,
Yao-Ting
Part Number: 66AK2H06 Hi
(i) I want to know how can i load DSPs (all four or any of them) from ARM and how will all cores communicate with each other i.e. communication between ARM cores and DSP cores , DSP cores and DSP cores?
(ii) Are all the peripherals…
Part Number: 66AK2H06 Hi, My customer is evaluating 66AK2H06 on their board. When using CCS, the most of initialization is done by GEL files. The gel file is attached. xtcievmk2x_arm.txt Customer is now trying to test without CCS and put most of initialization…
Part Number: 66AK2H06 Other Parts Discussed in Thread: 66AK2H14 Hi, This is additional question for the original post. Customer observed overshoot/undershoot on USBCLK. According to the original thread, USBCLK are not terminated until the software is…
Part Number: 66AK2H06 Hi, My customer wants to know the maximum downward pressure on 66AK2H06 package. The information is similar to one below in Intel website. https://www.intel.com/content/www/us/en/programmable/support/support-resources/knowledge…
Part Number: 66AK2H06 Hi, My customer is trying to use SPI boot with 66AK2H06. He refers to below document. Keystone II Architecture ARM Bootloader User Guide (SPRUHJ3) In section 2.7.1 GP Header Boot Image Format, there is below sentence. "A tool that…
Part Number: 66AK2H06 Hi, Customer wants to check UART boot function with 66AK2H06. They refer to below documents. http://www.ti.com/lit/an/spracn3/spracn3.pdf http://www.ti.com/lit/ug/spruhj3/spruhj3.pdf Questions: 1) Which UART pins are used, UART0…