Part Number: 66AK2H14 Hello
My custom board based on evmK2H is configured as follow
C66x core0 acting as PCI ROOT Complex, FPGA is endpoint
During PCI init, DSP open BAR1 (size 256 MB) starting at address 0x6000_0000 (this is DDR3B) and setup inbound…
Part Number: 66AK2H14 Hello Champs, 1. SDK 06.00.00.07, cmem-mod-4.16.00.00+gitAUTOINC+4f970f053b 2. insmod cmemk.ko, no phys_start paramters, set it in cmem_pools,phys_start=....dts ifle,
3. multiprocess test is ok. But when executing apitest, it prompted…
Part Number: 66AK2H14 On our custom board embedding a TI KeyStone II 66AK2H14, we would like to enable the last two NetCP Ethernet interfaces (netcp2 and 3).
We found some interesting settings in your Linux SDK documentation (please search netrx2 on …
Question 1: what is the purpose of txbclk_enable switch. Should it be set to '1' or '0'
Arun>> For 1G mode, txbclk enable should be set to 1. For 10G mode it can be set to 0. This is a tx byte clock mux select where it selects the PMA…
Hi Harish,
Harish Talanki1 said: 1. Is there a way to put down all DSP cores to power down mode by running code on ARM processor. We use vxWorks on ARM core.
2. Any boot-configuration changes like loading a specific register that could achieve this ? or…
Dear Customer,
Apologies for the delayed response and thanks for your patience.
Please go to the product folder -
https://www.ti.com/product/66AK2H14
and look at the "Design & development" and click software development. You will find SOFTWARE…
Part Number: 66AK2H14 Other Parts Discussed in Thread: FFTLIB , MATHLIB I am working on a phase 1 study for a program that needs to perform LU decomposition processing a Keystone II processor 66AK2H14 (not sure the part suffix). I'm trying to estimate…
Part Number: 66AK2E05 Other Parts Discussed in Thread: 66AK2H14 Hi, all
Now I have two board to compare the speed.
One board is the custom board which using 66AK2E05.The other is EVMK2H board which should using 66AK2H14
Both boards only run…
Part Number: 66AK2H14
Why are my posts/questions being locked and zero answers?
66AK2H14: What interrupt gets assert on CPTS time synchonization event when TS_INT_ENABLE is enabled? - Processors forum - Processors - TI E2E support forums
and
66AK2H14…
Part Number: 66AK2H14 I'm using XTCIEVMK2X ver4.0 board and trying to get the Mistrial RTM breakout card working for 10Gb ethernet. My initial test is trying to read the ES_SS_IDVER register but when I do I get a data fault. I've mapped the physical addresses…