Part Number: ADC-LD-BB
Hi Experts,
I know that ADC-LD-BB balun board is generally intended to use for single-ended-to-differential signal conversion with ADC1xDxx00RB. But is this also okay to use the other way around?
Please confirm. Thank you.
Regards…
Part Number: ADC-WB-BB The containerized ADC-WB-BB is a convenient packaging of the Minicircuit balun it uses. I am wondering if you offer a similarly packaged product, but using Mini Circuits or other baluns that extend down to .2 or .4 MHz.
Thanks! …
Part Number: ADC-WB-BB Hi TI,
Does the ADC-WB-BB board have any 3D/CAD model in STEP/IGES format?
I need to design it into my chassis along with other stuff.
Part Number: ADC-LD-BB How can i calculate the value of input capacitor to ADC-LD-BB balun transformer please give clear details with calculation formula
Part Number: ADC-WB-BB Other Parts Discussed in Thread: ADC-LD-BB I would like to know if this is compatible for my application. I have an 80 MHz 100 Ohm double ended signal that needs to go into the NI 6674T (which is single ended, 50 ohm). Will this…
Part Number: ADC-WB-BB Hi,
I have purchased two of these converters to measure the insertion loss of twisted pair telephone wire at different length. The result I am getting does not look anything I expect. For my testing I use a network analyzer (a spectrum…
Hi Given,
Your understanding with the busbar voltage range of the BQ79616-Q1 is correct. For the BQ79718-Q1 BB voltage range, you are also correct- however, the combined cell and BB voltage need to be within the measurable range of the CB ADC.
Best Regards…
Other Parts Discussed in Thread: ADC-WB-BB Hi,
I need to design a PCB with SMAs that match the pitch of two female SMAs (differential ends) of ADC-WB-BB as I plan to connect my PCB to ADC-WB-BB board using SMA male-male adaptors, without SMA cables.
Does…
Alfredo:
The TRF3711 may fit the requirements for you. The TRF3711-09 is a receiver demodulator. I understand that you only want the RF power detected, but the TRF3711 can do a good job of tuning to the specific CATV band within 400 MHz to 1500 MHz and…