Part Number: PCM3168A Other Parts Discussed in Thread: PCM3168 Hi,
I'm in a project where I need to have 6 different audio communication paths. I need each channel to be able to establish calls to one or several sip phones.
In A, i have an analogic…
Hello,
1) I have query regarding the absolute maximum input that the AFE7900EVM Rx input pin can handle with 0 dB DSA setting( with o dB attenuation) . As for the max full scale power range of the ADC is given up to 17.8 dBm for 30 MHz but here , DSA…
Hi Rob,
Refer to www.ti.com/.../adc-wb-bb
Before using balun, it is also fine to measure with single end with another port 50 Ohm terminated.
Regards,
Shawn
Hello Derek,
Hopefully my re uploaded diagram works.
I was hoping that you would be able to respond, I just didn't want to come across as demanding or dictating who should respond, if perhaps you and another of your colleagues shared the load. I do…
Part Number: ADC12J4000EVM Other Parts Discussed in Thread: TSW12J54EVM , ADC-WB-BB , , LMH5401 , ADC12J4000 , TSW14J57EVM Hi Jim
My input signal is from 10MHz to 400MHz, if this board work in 1GSPS mode, will my low frequency component pass into the system…
Part Number: LMK04828BEVM Other Parts Discussed in Thread: ADC-WB-BB , DAC3484EVM , CDCE62005 , DAC3484 , CDCM7005 I'm driving out 1 1Vpp 153.6MHz LVPECL20 +/- signal from CLKout0/CLKout0* and connected to a ADC-WB-BB balun that connects to the J9 CLKIN input…
Part Number: BEAGL-BONE-BLACK Hello,
we are trying to use a BELA audio cape with a BB and are writing our own code to test the ADC on board the cape (AD7699). We are using the PRU to synchronize timings and are seeing some issue with the SPI bus. The…