Part Number: ADC08060EVM Hi. I have an ADC08060EVM connected to a TSW1400. Everything seems to working ok (High Speed Data Converter reports values) but I cannot get the ADC output value to change. Setting JP8 and JP9 on the ADC to pins 1-2 means I get…
Hi William,
I have done some testing on the ADC08060EVM, and have the following results.
10 MSPS: 1 MHz input (band-pass filter): ~46 dBFS SNR and ~61 dBFS SFDR
60 MSPS, 1 MHz input (band-pass filter): ~46 dBFS SNR and 60 dBFS SFDR
Best Regards…
Hi Fax
The best fit for that need is probably the ADC08060. It is active and the recently updated ADC08060EVM is available for customer evaluation.
While the ADC1173 is only rated for -40 to +75 C operation the ADC08060 is rated from -40 to +85C.
Best…