Part Number: ADC08DL502 Other Parts Discussed in Thread: ADC08D502 Hello, I would like to interface an ADC08DL502, using 1.8V supplies for VA and VDR, to a Xilinx Artix-7 FPGA. I noticed that the ADC08DL502/ADC08D502 LVDS outputs' differential voltage specifications…
Part Number: ADC08D500 Other Parts Discussed in Thread: ADC08D502 , Hi team,
Both ADC08D500 and ADC08D502 different are D500 can interleave to 1GBPS per channel but D502 only 500MBPS.
Besides both device performance are same? thanks!
Part Number: ADC08D502 Other Parts Discussed in Thread: ADC08D500 Hi team,
When I read the ADC08D502 datasheet, it said it's a Dual 8-Bit, 500 MSPS A/D Converter. I noticed that it has 2 ADC cores inside the chip. So my question is what's the definition…
Part Number: ADC08D502 Other Parts Discussed in Thread: SN74AVC4T774 Hi,
Customer query below.
I’m just going over how we’re going to connect it to an FPGA. Unfortunately, the ADC08D502 seems to use quite non-standard input thresholds on the digital inputs…
Other Parts Discussed in Thread: ADC08D502 , ADC08DL502 I see the lower power and cheaper "DL" even is specced with a higher analog BW.
The dynamic performance SINAD limit may be 2 dB worse for the "DL", but the higher Analog BW and lower power…
Other Parts Discussed in Thread: ADC08D1520 Dear !
I wanted to ask some advice to design high speed adc:
- Draw PCB
- Get data high speed
- buffer for data
thanks!
Other Parts Discussed in Thread: ADC08D502 , ADC08D500 If I connect the two inputs of ADC08D502 together and apply 500Mhz clock input , can I have 1G sampling rate upon using DDR clocking ??
Part Number: ADS4229 Other Parts Discussed in Thread: ADC08D502 Hi team,
Let me double-check if the dual channel of ADS4229 can make a conversion simultaneously. (As a background, I'd like to get a high speed data in parallel.)
ADC08D502 looks to have…
Hi Dan
To have the fewest number of output buses for a 6 input 500MSPS system, the best solution is to use 3x ADC08D1020 with the devices operating in non-demux output mode and with a 500 MHz clock. There will be six 8-bit output data buses. If they need…