Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Wally,
Are you experiencing an incompatibility other than the name 'ADS62P23' is not available in HSDC Pro?
Will you please try selecting 'ADS62P43' in HSDC Pro and try to capture data? The scale should be off because the software expects a 14…
Other Parts Discussed in Thread: ADC10080 , THS7353 , THS7303 Hi Team,
Please advise me proposing a solution for a HD Video A/D conversion.
In order to fully utilize the ADC10080 dynamic range, it is necessary to make coincide pedestal level (Back porch…
Other Parts Discussed in Thread: ADC10080 , ADC10040 , LMH6550 Hi Team,
Please allow me to ask you question about admissible load to VREFB and VCOM pin of ADC10080.
I understand ADC10080 recommends not to connect loads to these pins, however, customer would…
Other Parts Discussed in Thread: ADC10080 , OMAP-L138 Hi,
For a new opportunity at our customer, they would like to interface the ADC10080 to the TI: OMAP-L138 (DSP+ARM Processor). Meprolight would like to use the OMAP’s Universal Parallel Port (upp…
Hi Shyam
Most of the ADCs that have the required resolution and sample rate are not directly compatible with the 2V common mode voltage of your sensor.
Would it be OK to use a fully differential amplifier in between the sensor outputs and ADC inputs,…
Hi Satoshi
The Vcom output has very little current drive capability. Please see this previous E2E post addressing the same question for the ADC10080 (higher speed version of ADC10065).
https://e2e.ti.com/support/data_converters/high_speed_data_converters…
Other Parts Discussed in Thread: ADC10080 , WAVEVISION5 Dear Specialists
My customer is considering ADC10080 and confirm the spec by ADC10080EVAL and WAVEVSN-BRD-4.4.
The customer wants to convert 100-1000us interval and 20us sampling.
Is the EVAL possible…
Other Parts Discussed in Thread: ADC10080 , ADC10040 , ADC10065 , THS4509 I would like to design a board similar to the ADC10080 EVM that will contain some added circuitry and will interface to the WaveVision (like the ADC10080 EVM ).
What is the function…
Yu,
I support the ADC10080. I am not intimately familiar with the uPP interface, but I have made the following observations:
- The uPP interface signals are: DATA, CLOCK, WAIT, ENABLE, START. The OMAP-L138 datasheet mentions that the use of ENABLE, WAIT…
Hi Sunil,
I need to close my design...
Do you think the ADS5237/ADC10080 can connect to the uPP at >65MSPS?
Is there any application note or reference design on that matter ?
Regards.