Part Number: ADC10D1000 Other Parts Discussed in Thread: ADC12D1000 Hi TI experts,
I have some technical questions on ADC10D1000, as listed below.
1. I see Vcmo is internally buffered. Does TI recommend connecting this pin directly to the common-mode…
Part Number: ADC10D1000 Other Parts Discussed in Thread: ADC12D1600
hello,
what is the mass of the following ADCs please:
08d1520
10d1000
12d1600
14155
thank you
Part Number: ADC12D1800RB I have just unboxed the ADC12D1800RB/NOPB. Following the installation instructions, I am unable to install the ADC10D1000 USB driver.
Running Windows 10 Enterprise as an administrator. Have successfully installed WV5 5.0.6.465…
Part Number: ADC08500 Other Parts Discussed in Thread: ADC09SJ800 , ADC10D1000 Hi,
Do we have an IBIS model for ADC08500CIYB/NOPB? I couldn't find it on ti web.
Thanks,
Chuchen
Other Parts Discussed in Thread: ADC10D1000 Hi
In the ADC10D1000 datasheet (page 19) the Vcmo Lim tolerances are stated as 1.15V and 1.35V, Vcmo nominal 1.25V. Temperature coefficient of 38ppm/C is also given
Why are the Lim tolerances so big (1.15V to…
I need some questions answered on the evaluation boards in reference to these parts and if using the boards along with the system software will allow us to test and validate them against the data sheet. The evaluation boards look like they support a socket…
Part Number: ADC08D1520RB Other Parts Discussed in Thread: WAVEVISION5 , ADC10D1000 ,
Is an SDK available for ADC evaluation boards? Is WAVEVISION5 open source?
Hello everyone,
I got another non-rectangular ADC10D1500RB. It doesn't works neither. This is 3rd time.
On the other hand, I could test ADC08D1520RB and it seems successfully connected with WaveVision5.
The ADC08D1520 is shown up as "ADC10D1000" in…
Part Number: WAVEVISION5 Hello
The Hardware I'm using is the ADC10D1000-rb.
I've been using the wvdll.dll in python 3.71(32-bit) on windows 10 and I will get strange crashes when working with it.
I was hoping that since there isn't anymore active…
Other Parts Discussed in Thread: ADC10D1000 , ADC12D1600 Hi,
We are using the ADC12D1600QML. Is there a "daisy chain" package for assembly qualification and testing?
Thanks,
rich :-)