Hi David
The document below has some characterization information on the ADC10D1000 thermal diode. This previous generation device uses the same diode, the same package and the same semiconductor process as the ADC12D1800RF.
4747.ADC1XD1XXX Thermal…
Other Parts Discussed in Thread: ADC10D1000
Hello,
I am using the ADC12D1600RFRB for digitizing signal in continuous time interval of 10msec. For this purpose I use memory capture platform Xilinx ML-605, which has sufficient on-board memory to…
Other Parts Discussed in Thread: ADC10D1000 Dear Sir/Madam,
I’m Nick from DSO National Laboratories. I’m interested in the follow product: ADC10D1000QML and ADC10D1000
There are queries which need inputs from the company.
1) Is this part(ADC10D1000QML…
Other Parts Discussed in Thread: ADC10D1000 , WAVEVISION5 Hi,
Which cpp script files are used for the adc08d1520rb? I could not find anything bearing the name of the ADC.
Regards,
Supratim
Other Parts Discussed in Thread: WAVEVISION5 , ADC10D1000 I wonder what is the model of Xilinx Programmer JTAG cable working with ADC08D1520RB to allow us to load new FPGA image on the board without causing conflict.
Thank yoU!
Best Regards, …
Hi Carletta
NOPB indicates a "no lead" or "no Pb" product. This is a terminology used in the National Semiconductor component ordering systems to indicate which products are in lead free packaging. Most products are lead-free, but some are available…
Part Number: WAVEVISION5 Hello
The Hardware I'm using is the ADC10D1000-rb.
I've been using the wvdll.dll in python 3.71(32-bit) on windows 10 and I will get strange crashes when working with it.
I was hoping that since there isn't anymore active…
Other Parts Discussed in Thread: LM95213 , LM95233 , ADC10D1000 Hi,
I'm doing a design with the ADC12D1600QML-SP . Is there any information on the tdiode_p/n pins? A recommended circuit?
The data sheet recommends using the LM95213 but I can't find…
Other Parts Discussed in Thread: ADC12D1600RB , ADC10D1000 Hi, Jim
I have some issue with the ADC12D1600RB.
After installing the software and the hardware, I followed the user's guide and started the WV5. But it showed that a hardware error has occurred…
Other Parts Discussed in Thread: WAVEVISION5 , ADC10D1000 Hello
I took FPGA source code from ADC12D800RFRB Design Package and found that after synthesize and creation "Generate Programming File" on ISE Project Navigator, i cant program my FPGA. i have…