Part Number: ADC10D1500 Hi TI expert
We are planning to use the part ADC10D1500 in our design at maximum possible frequency.
Please provide the analog input power loss vs frequency data. It is said that FPBW is 2.8G where the power would be 3dB less…
Part Number: ADC10D1500 Does the ADC10D1500CIUT termination finish meets the solderability requirements of IPC/JEDEC J-STD-002 for components and wires?
Hi Arunkumar,
Sure I am happy to demo your board and understand a bit more. I will take this offline and send you an email to schedule a conference call/meeting.
Regards,
Rob
Hi Jim,
Thank you for the replay...
We have reduced the Full Scale Range setting to 790mV and tested. I have also tried on command calibration of the ADC using CAL Pin. But there is no change in the result.
I am attaching the schematic with this…
Hi Dongjin,
As I mentioned in previous e2e post if you want to measure low frequency signal (100Hz) you cannot use the balun. You will have to use single-ended to differential amplifier which is DC coupled and is set to common mode voltage requirements…
Other Parts Discussed in Thread: ADC10D1500 Hi,
Customer wants to obtain 1/4 digital output of ADC sampling rate from 1 analog input.
For example,
ADC10D1500 sampling rate is 1.0Gsps and use 4 parallel LVDS output.
As figure.7 in page 34 in the…
Other Parts Discussed in Thread: ADC10D1500 Hi,
Customer would like to have SI for ADC10D1500.
For eye mask, LVDS timing spec is needed.
Could you provide it?
In the datasheet, there is only voltage spec of LVDS.
Thanks.
Hi Neeraj,
Coming back to this issue with the insertion loss, does TI recomend any solution (amplifier/equalizer) to be used with the ADC10D1500 operating in DESIQ mode? Our system must work for a very wide input bandwidth and the insertion loss between…
Hi Heedo,
I have attached the excel file which show the transfer function of an 8 bit ADC. The first column shows offset binary value (data) coming from the ADC. Second column show the equivalent decimal number for each binary code. The third column…