Part Number: ADC122S021ADC122S021_fail.pdf
With a new lot of produced PCBs we see a failure with the ADC122S021, which previous were working OK (same PCB, same SW).
As can be seen on attached file, an extra tracking pulse is required, which gives…
Michael, thanks for your answer.
I checked pin 5 to better than 1mV precision. The signal is also clean from glitches. My scope has 350MHz BW (Agilent MSO-X 3034A). When preparing my post I paid attention that the clock has a rise/fall time of 25nS,…
Other Parts Discussed in Thread: ADC122S021 Hi,
I have built up a design generated from the WEBENCH for K-type generic grounded thermocouple enclosed herewith using ADC122S021.
I am able to achieve analog voltage from both channel IN1 and IN2 .
…
Other Parts Discussed in Thread: ADC122S021 Hello,
My customer uses the ADC122S021 and has a question.
Q) Is there a internal pull up in the CS pin ?
Regards,
Naoki Aoyama
Part Number: TLV2542 Other Parts Discussed in Thread: ADC122S021 We are using TLV2542 in our design, We tried giving MUX reset cycles 4 to 7 clocks with CS low.
We are repeating these 4 bit cycles for 5 time - so that at once the MUX will get RESET…
Hi Shwetha,
I could not find a single channel ADC with Linux driver support. The ADC122S021 is a dual channel ADC that is supported by the ADC128S052SW-LINUX driver.
Regards,
Chase
Part Number: ADS112U04 Other Parts Discussed in Thread: LMP7732 , ADC122S021 Hi team
A customer is dealing with a design with thermopiles application and is considering the ADS112U04.
He noticed that the DS mentions thermocouple as the recommended…
Hello,
I did a quick parametric search that resulted in 10 devices
I would recommend the ADC122S021 , this is a 12 bit device, but with oversampling you can get a 14 bit resolution if necessary.
There is also the ADS7280 which is 14 bits.
Regards…
Hi Phil,
It doesn't seem like we have any 4 input channel device that has such large pad spacing. This 1 channel part, ADC121S021 , has a spacing of 0.45mm. There is also this 2 channel part, ADC122S021 .
Out of curiosity, what is your project application…
Part Number: ADC121S021 Other Parts Discussed in Thread: ADC122S021 , ADC124S021
Hi Team,
I want to know software compatibility of ADS12XS021 series.
Are following devices register compatible?
ADC121S021 ADC122S021 ADC124S021
If not, please…