Part Number: ADC128S102 Hello,
Happy new year!
It's the first time our customer use the ADC128s102, our customer want a configuration example about ADC128S102' SPI telecommunication sampling. They used the regular IO port SPI.
I wonder if there…
Part Number: ADC128S102 Is the minimum sample rate 50 ksps for this part? I know it is for the -SP space version of this part.
The data sheet is confusing, it says the minimum sample rate (continuous) is 500 ksps and typical sample rate (continuous) is…
Part Number: ADC128S102 Other Parts Discussed in Thread: ADS7952 Hi team,
I used cross-reference to find ADC128S102 to replace AD7928BRUZ-REEL7.
Is the solution suitable? or have another better solution? thanks
Part Number: ADC128S102-SEP Other Parts Discussed in Thread: ADC128S102QML-SP , Hello, According to the application note, ADC128S102QML-SP Application Advisory, the ADC128S102QML-SP may exhibit code errors called sparkle codes at the output of the device…
Part Number: ADC128S102-SEP Other Parts Discussed in Thread: ADC128S102 if my ADC have 6 channel with mux , if i confirm any one of the channel dnl & snr is fine. i can say remaining channel also similar behaviors ?
Part Number: ADC128S102 I am planning on using the ADC128S102 in a design that has relatively tight accuracy requirements over temperature, but not that stringent of resolution requirements.
No need to recommend alternate ADC p/n's I am pretty set on…
Part Number: ADC128S102 Hello,
We’re using the ADC128S102 with VA at 5V and VD at 3.3V. There is a potential for the 5V to be delayed by 3ms. The datasheet for the ADC128S102 has a note regarding power sequencing that says “care must be taken to…
Part Number: ADC128S102-SEP in the Annex (pag.5 and following) the measured parameter are not clearly decribed, in particulat test conditions. The name of the parameters suggest some test conditions, but it is not clear.
Example:
DNL_MAX_16M_5V (page…
Part Number: ADC128S102 Is there a specification for the minimum or maximum input rise time of this device? I did not see one in the datasheet, and the timing diagram only shows the delays between edges on different signals.