Part Number: ADC128S102 Hi there,
I am using the ADC128S102WGRQV. In the part datasheet in section 7.3.2 it is recommended to keep the input resistance to <100 Ohm. However with such a low external resistor value we won't be able to limit the ADC internal…
Part Number: ADC128S102 Hi,
I am accessing the ADC128S102 over a SPI interface. When I look at the DOUT line, it doesn't seem to make sense to me (see photo).
The device is running off 3.3V. I see a 3.3V pulse but it is happening when 0s are supposed…
Part Number: ADC128S102
I read from ADC128S102. The diagram is following
SPI settings CPOL = 1, CPHA = 0
SPI MaserIn - pin DOUT
SPI MaseOut - pin DIN
SPI CLK - pin SCLK
ADC SS10 - pin CS
s_adc_latched val - is the value on a current channel
As you…
Part Number: ADC128S102-SEP I want to check for this part ADC128S102PWTSEP, if it has a cavity inside, to see if we need to do a PIND test or not.
Please advise,
Thank you very much,
Salwa
Part Number: ADC128S102-SEP Other Parts Discussed in Thread: ADC128S102 Hi,
Could you check expected error case with abnormal ground?
When 3.3V or 5V is on GND, damage of ADC128S102 is expected according to the datasheet absolute maximum.
The question…
Part Number: ADC128S102 We can possibly have a condition where we would be applying -3.6V to the analog input of an unpowered ADC128 through a 3.3K resistor (1.1mA). Is this allowable? We could also possibly have a condition +3.6V through a 10K to an…
Part Number: ADC128S102-SEP I'm looking for the shock and vibration rating for ADC128S102-SEP (TSSOP package) full part number is ADC128S102PWTSEP.
Thanks
Part Number: ADC128S102 Hi,
I see in the datasheet it list the minimum SCLK frequency as 8MHz and the maximum frequency of 16MHZ. It also list the typical of 800KHz.
Am I to assume that Ti recommends that you should operate this ADC in the 8-16MHz range…