Part Number: ADC128S102-SEP Other Parts Discussed in Thread: ADC128S102 if my ADC have 6 channel with mux , if i confirm any one of the channel dnl & snr is fine. i can say remaining channel also similar behaviors ?
Part Number: ADC128S102-SEP in the Annex (pag.5 and following) the measured parameter are not clearly decribed, in particulat test conditions. The name of the parameters suggest some test conditions, but it is not clear.
Example:
DNL_MAX_16M_5V (page…
Part Number: ADC128S102-SEP I want to check for this part ADC128S102PWTSEP, if it has a cavity inside, to see if we need to do a PIND test or not.
Please advise,
Thank you very much,
Salwa
Part Number: ADC128S102-SEP Other Parts Discussed in Thread: ADC128S102 Hi,
Could you check expected error case with abnormal ground?
When 3.3V or 5V is on GND, damage of ADC128S102 is expected according to the datasheet absolute maximum.
The question…
Part Number: ADC128S102-SEP I'm looking for the shock and vibration rating for ADC128S102-SEP (TSSOP package) full part number is ADC128S102PWTSEP.
Thanks
Part Number: ADC128S102-SEP Hello - I have reviewed the reliability information on-line ( https://www.ti.com/quality-reliability-packaging-download/report?opn=ADC128S102PWTSE ), but I cannot find the thickness of the gold in the leads. What is the thickness…
Part Number: ADC128S102-SEP Hi Expert,
My csutomer want to know the semiconductor manufacturing process node about ADC128S102-SEP.
I think it may be in the range between 65nm~300nm, am I right?
Thanks.
Part Number: ADC128S102-SEP In the datasheet, it is mentioned that analog power rail should ramp before digital power rail during power up.
What about during power down? Is there guidance about proper sequencing? Should digital power rail ramp down first…
Part Number: ADC128S102-SEP Other Parts Discussed in Thread: ADC128S102 Hello,
We have an application where the analog inputs are active before the power up of the analog supply (Va) is complete. What are the implications of this condition and how can…