Part Number: LM124A Other Parts Discussed in Thread: ADC128S102 , , OPA4991-EP , TLV2374-EP , TLV9004 , , OPA4991 , OPA4H199-SEP Tool/software: hello. I implemented OPAMP LM124A as a voltage follower and designed to monitor each power source through ADC128S102…
Part Number: AFE11612-SEP Other Parts Discussed in Thread: ADC128S102-SEP , DAC5675A-SP , While analyzing the IC datasheet and comparing it with the other ADCs and DACs available in the TI product selector list, some queries were raised.
Kindly provide a…
Hello,
I'm assuming that your supply voltage will be 5V. The 10mA current max is due to an internal ESD diode present on the analog input to analog supply that protects from overvoltage conditions at the analog input. This diode has a nominal typical…
Hi Anthony,
1. The voltage won't really be the main issue, but the resulting current can damage internal structures of the device. It still would not be recommended to exceed the voltage maximum ratings, but limiting the current is the real concern.…
Part Number: TPS73801-SEP Other Parts Discussed in Thread: TPS73801 , ADC128S102-SEP , ADC128S102 , LMX2694-EP , LMX2694-SEP To Whom It May Concern,
Hope you're well.
Please allow me to submit inquiry as below.
<Inquiry>
Are the same Si chips…
Hi,
Thanks for your question. The closest device is the ADC128S102-SEP 8 channel, 50ksps to 1MSPS device in the same family. It is radiation tolerant and has an operating temperature range of –55°C to 125°C.
Best,
Samiha
Part Number: ADC128S102QML-SP Other Parts Discussed in Thread: ADC128S102 Collin Wells replied in the post ADC128S102-SEP: Can I apply input signals before the analog supply (Va) with a partial circuit diagram of the ESD Protection Diodes within the ADC128S102…
Thank you for getting back to me.
One question though, is the minimum sample rate 500 kHz or 50 kHz?
The reason I ask is because the ADC128S102-SEP (rad-hard part) has a minimum sample rate of 50 sps (would you verify that though). It's sample rate range…
Hello,
You can use the SPICE model available for the ADC128S102-SEP, this will apply the same as for the catalog device
https://www.ti.com/product/ADC128S102-SEP?keyMatch=&tisearch=search-everything&usecase=partmatches#design-development
rega…
Hi Rajan,
I wanted to add to Keith's nice response that we have a video which explains these effects in detail and also a tool in our analog engineer calculator which can be used to help with your designs.
https://www.ti.com/tool/ANALOG-ENGINEER-…