Part Number: ADC12D1600 Hello,
I plan on using the ADC12D1600 for a custom board design. I would like to use this device as a dual channel ADC with 1.6 GHz sampling speed per channel. One problem is that the FPGA to which this device interfaces with…
Part Number: ADC12D1600 Other Parts Discussed in Thread: ADC12D800RF , , , ADC12D1620QML-SP Hello,
I am just wondering if anyone has tried to simulate the IBIS model of this component in ADS.
Thank you
Part Number: ADC12D1600 Hi
If DNC pin of ADC12D1600 is shorted to power rail or Ground? What will happen? Could you briefly explain?
Regards,
Aravindhan R
Part Number: ADC12D1600 Hi team,
Customers use PIN mode to control ADC12D1600, In Demux Mode, Non-DES Mode, power-on calibration, use test pattern, according to the datasheet description, test pattern will have a continuous 010. Now the data DI captured…
Part Number: ADC12D1600 Hi
I have doubt on ADC Power and GND section.This ADC12D1600 IC has more power and Gnd pins.Is these all the pins are redundant for handling limited current? or each power pin is meant for particular driver of the IC. I want…
Part Number: ADC12D1600 Other Parts Discussed in Thread: ADC12D1800 Hi -
Please could I get an accurate pin assignments table (csv/xls) ? Your ultralibrarian file is incomplete (e.g. pin J17 label is "J17").
Thanks, David
Hi Drac82,
The max output data rate for the ADC12D1600's LVDS bus can handle is 1Gbps.
So please use the 1:2 Demux Non-Des mode.
Especially when clocking ADC12D1600 at full rate.
Hope this helps.
Regards,
Rob
Part Number: ADC12D1600 Hello,
Is there information available with respect to pin-package delays of the ADC12D1600CIUT? I want to use this information for the PCB layout to minimize the skew between the LVDS lines (clock and data).
Kind regards, …