Part Number: ADC12D1620QML-SP Other Parts Discussed in Thread: ADC12D1600 , ADC12D1800RF , ADC12D1000 , ADC12D1600QML-SP On page 38 of the specification, in the Output Control and Adjust section of Table 1, the DDR/SDR selection is done by the SDR bit…
Part Number: ADC12D1600QML-SP Other Parts Discussed in Thread: ADC12D1600 , ADC12D1620QML-SP , If you look at the commercial ADC12D1600 data sheet, dated Aug 2015, the absolute maximum ratings table specifies says "voltage on any pin (except Vin+/-)"…
Hi Amanda
You are correct, if the customer wants to double the sample rate and corresponding output data rate, then they need to migrate from the ADC12D1000 to the ADC12D1600. The ADC12D1000 max clock rate is 1000 MHz. The ADC12D1600 will support their…
Hi,
Thanks for the quick response, really appreciate your time.
Do you have any information on the resistor itself? I am interested in the part stress analysis if one exists. If not, can you tell me what technology the ADC12D1600 part was fabricated…
Part Number: ADC12D1600QML-SP Other Parts Discussed in Thread: ADC12D1600 , , ADC12D1600RF The commercial version of the ADC12D1600 has a Vcmo pin which, when grounded allows AC coupled Vin adjusted to the common mode level internally. When not grounded…
Other Parts Discussed in Thread: ADC12D1600 , LMH5401 , LMH5401EVM , WAVEVISION5 Hi
I buy a ADC12D1600RFRB. I saw the adc12d1600 Datasheet .the Electrical Characteristics: Analog Input/Output and Reference,I noticed when NON-EXTENDED CONTROL MODE,the…
Other Parts Discussed in Thread: ADC12D1600 , ADC12J2700 , ADC12D500RF , ADC12J2700EVM Hello,
I am searching new ADC for new project, which has variable clock source range(270MHz to 450Mhz).
Our input source is correlated with this variable clock…
Hi,
Yes you should be able to use ADC12D1600RF instead of ADC12D1600 without any problems. The main difference between the two is ADC12D1600RF has new mode of operation called DESCLKIQ. 1-2dB improvements in the noise floor, linearity improvements…
Other Parts Discussed in Thread: ADC12D1600 , ADC10D1500 Hi,
I have the ADC1xDxxxx(RF)RB board configured for the ADC12D1600 (our target part for our design).
The schematic shows that on each of the 4 output data buses, there are two sets of three…