Part Number: ADC12D1600RFRB Hi Experts,
I setup WAVEVISION 5 and drivers for Win10, and power up ADC12D1600RFRB with 12Vin from power supply.
but WAVEVISION 5 does not capture any hardware device after EVM power up.
The attached files are what I referred…
Part Number: ADC12D1600RFRB Hi Team, Our customer would like to request for the whole length and width dimension of ADC12D1600RFRB board.
Can you share it? Thanks! Jonathan
Hi Phil
There may be a firmware that will work for the customer. Have him try the following steps:
Navigate to C:\Program Files (x86)\National Semiconductor\WaveVision5\hardware\fpga_images
Rename adc10d1000_xc4vlx25_adc12d1600rfrb.bit to adc10d1000_xc4vlx25_adc12d1600rfrb…
Hi Jiaxiang
The LMH5401EVM VCMI should be connected to VCMO, which is available at pin 9 of J17 and pin 9 of J15.
You will also need to change the ADC from AC-coupled mode to DC-coupled mode. The default configuration has VCMO connected to ground at TP5…
We are connecting an ADC12D1600RFRB with a Xilinx Kintex-7 development board KC705 using the FMC connector. We are using the ADC in DES mode and would like to adjust the ADC settings over the FMC bus. Is there any reference code available for this?
Other Parts Discussed in Thread: LMX2531 I have an ADC board ADC12D1600RFRB that I want to sample on 1200MHz. How do I put the PLL at this frequency? According to the users' guide, the PLL can only be programmed in the range 1530-1636MHz. I would like…
Hi Andreas,
I think that with Matlab you should check the "Enable continuous mode". Doing this, GHzADC software will write data files to c:\TclApps\GHzADC\Output\ folder, were it usually put the channel I and Q data files. Matlab is reading the files…
Part Number: ADC12D1600RB Other Parts Discussed in Thread: WAVEVISION5 Hi there,
I've got a few questions about the ADC12D1600RB.
· Is the ADC12D1600RB S/W (WaveVision) compatible with Windows 10 20H2 ?
· Can WaveVision export sampled…
Hi Barbara,
The board dimensions are 4x4.25 inches.
Is there a reason you plan to use this board/interface to a logic analyzer?
Both the ADC12D1600RFRB/1800RFRB EVMs are supported via a USB connection and Wavevision software, which can capture and display…
Other Parts Discussed in Thread: ADC12D1600RB Will the ADC12D1600RFRB work when interfaced with a VC707 Virtex-7 eval board? As I understand it some FMC cards that have been designed for a Virtex-5 board may not be compatible with a Virtex-7 board.
Thanks…