Part Number: ADC12D1620QML-SP Hello,
Looking at the Figure 3 of AN-2132, DCLK could be four different phases in unsyncronized DCLKs and Demux Mode. Does this mean, tOD could actually be the specified value (typ) in the datasheet + either 0 degree, 90…
Part Number: ADC12D1620QML-SP Hello,
I am evaluating two TSW12D1620 eval boards. I am a seeing a fixed -50dBm spur at 400MHz on both cards with or with a the 1.6GHz clock inputted which make me feel it is something I have wrong in my setup. I am following…
Part Number: ADC12D1600QML-SP Other Parts Discussed in Thread: ADC12D1620QML-SP , If I have a circuit board that has been fabricated for the ADC12D1620QML-SP, under what conditions, if any, can I use the ADC12D1600QML-SP in its place?
Part Number: ADC12D1620QML-SP Other Parts Discussed in Thread: ADC12D1600 Do we have any guidance on total latency over temperature or lot-to-lot variation? Even a ballpark would help us make sure everything will be fine.
Part Number: ADC12D1620QML-SP Hello,
I am evaluating the ADC12D1620QML-SP using the TSW12D1620 with the TSW14DL3200 eval boards. My question is when I obtain the .csv output file of the data I see some statistics are displayed and want to know the meaning…
Part Number: ADC12D1620QML-SP Good afternoon,
We are enabling the test pattern mode through the SPI registers, using bit 12 of configuration register 1. What is the expected time between enabling the test patterns to actually seeing the data at the…
Part Number: ADC12D1620QML-SP Other Parts Discussed in Thread: LMX2615-SP What voltage is the Vbias for the ADC CLK+/- inputs to the ADC12D1620? Is it the same as VCMO = +1.25V?
Part Number: ADC12D1620QML-SP Hi Team,
Customer has question regarding ADC12D1620QML-SP. Below is the inquiry.
"
In terms of output modes, it appears that there are I and Q outputs, is there a mode where we can use only I and it will contain all…