Other Parts Discussed in Thread: ADC12D1800RF , ADC12D1800 Hi
I would like to know if ADC12D1800RF is using the same DIE as ADC12D1800? What's the difference between these two ADCs?
Thank you!
Bin Liang
Other Parts Discussed in Thread: ADC12D1800RF I have an ADC12D1800RF card that I would like to use for sampling a ~1GHz wide IF band centered at fc=3.0GHz (ie. 2.5 to 3.5 GHz).
I am assuming I should use Fs=3.6GHz and 2nd Nyquist band.... or should I possibly…
Hi,
I understood about DESIQ mode.
But, i wonder when DESIQ mode use.
What are the benefits of DESIQ mode ?
- Customer : Nextwill (www.nextwill.com)
- App : Communication Equipment.
- Q'ty : 100 over.
- MP : Q3.2015
Thnaks & regards.
Other Parts Discussed in Thread: ADC12D1800 , ADC12D1800RF Hi,
we evaluated adc12d1800 in the past. Now we are evaluating adc12d1800rf now. We have some questions,
1. What is the difference between adc12d1800 and adc12d1800rf?
2. Can the users migrate from…
Other Parts Discussed in Thread: ADC12D1800RF Hi,
I would like to ask you some questions regarding the product ADC12D1800RF, which I am trying to model in Simulink: 1)a) In the data manual, the noise floor density is given by -154.0 dBFS/Hz. I would…
Other Parts Discussed in Thread: ADS5400 , ADC12D1800RF What happens if the clock is faster than 1800 MHz? How far could it be pushed to still produce a low error data stream?
Would active cooling and supply voltage altering help? Has anybody here tried…
Other Parts Discussed in Thread: ADC12D1800RF , ADC12D800RF , ADS5400 , ADC12D500RF , ADC12D1800 Hi,
I am using the EVB for the ADC12D1800RF, and noticed a problem with the HD3 performance:
sampling rate is 1800MSPS, with test signal at 124MHz.
when signal…
Hi,
I would like to find out the process technology of the 3.6 GSPS ADC, ADC12D1800RFIUT-12 and also if the part is GaAs, GaN or CMOS etc?
Thanks,
Kwan
Other Parts Discussed in Thread: LM95233 , ADC10D1000 , ADC12D1800RF The datasheet states that the temperature sensor diode has not been fully characterized. What information is available for the diode?
I would like to monitor the die temperature without…
Other Parts Discussed in Thread: ADC12D1800RF Hi
Please let me confirm some questions about ADC12D1800RF.
Qestion Are there any input pin that must not be left floating at power-on ? (In the case of floating, is the destruction possible?)
Best Regards, S…