Part Number: ADC12D1800RFRB I am in need of a compatible data capture card for the ADC12D1800RFRB at speeds greater than 1GSPS. Would something like the TSW1400EVM work?
Part Number: ADC12D1800RFRB Hello,
We are using the ADC12D1800RFRB. Using external logic analysis, the data output rate, DQ , appears to be 1/4 of the input frequency in non-DES mode. While in DESI-mode we appear to be getting 1/2 of the input frequency…
Part Number: ADC12D1800RFRB Hello,
We are using the ADC12D100RFRB. My question is: How can we bypass the on board voltage regulators so we can attach an external power supply in order to provide our own biasing voltages?
Thanks,
Edgar
Part Number: ADC12D1800RFRB Hi
I am using ADC12D1800RFRB Evaluation Board.
I have configure the on board PLL for 1.8 GHz clock...So I am sending sampling frequency 1.8GHz to adc.
I have configured the adc as following:
NDM <= '1'; (non demux…
Part Number: ADC12D1800RFRB Hello,
We are using the ADC12D1800RFRB and have attached a board we designed in order to get the output onto an oscilloscope. We are however, having difficulty getting the bits to display, so we are assuming the output data…
Part Number: ADC12D1800RFRB Dear all,
I currently use the ADC12D1800RFRB with the ML605 board for a continuous data capture.
My problem is, when I make some separate captures, with a reset of the ML605 board between each, all my captures are fine.
However…
Part Number: ADC12D1800RFRB Hi,
For a LIDAR application I need to record GHz resolution waveform traces about 100 microseconds long, where I'm expecting 1000 events per second. The API provided for this ADC evaluation board seems to allow this, except…
Part Number: ADC12D1800RFRB
Hello,
We are using the ADC12D1800RFRB. When switching to an external clock the over-range LED turns on for both channels without the clock having been turned on. Even when the clock is turned on, the LED still appear to be…
Hi,
I am trying to figure out the time order of the of ADC output from IDDR. I attempted to get the order from this section of the comment in the acd12d10000_rfrf.v file.
/* The time order for des mode (above) is: (example for 8 bit adc) * dqd1_reg[7…
Other Parts Discussed in Thread: WAVEVISION5 , ADC12D1800 , ADC10D1000 hi
i have 3 pcs of ADC12D1800RFRB which i signed #1,#2,#3. #1 was bought 2 years ago, and i can use it correctly following the < wavevision5 software User’s Guide.pdf >.
…