Part Number: ADC12DJ3200 Hi team,
One of our customer's issues, I'm forwarding it below, could you please provide some troubleshooting suggestions
ADC set to JMODE1 mode, lane_rate=6.4G ,K=4 , jesd204B_core lck=160MHz, sysref is both 20MHz, using…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: LMK04828 , , TSW14J57EVM Hi team,
The ADC model is ADC12DJ3200 and the PLL is LMK04828.
The ADC sampling rate is 5 GSPS, the sampling clock provides 2.5 GSPS, and the sysref is 3.90625 MHz, in pulse…
Part Number: ADC12DJ3200 I want to know the digital value of Input Full Scale on the AD12DJ3200(JMODE16) xilinx FPGA Chipscope.
Please check if there is anything missing in ADC setting or getting digital value.
1. Device: AD12DJ3200
- JMODE 16 (Dual…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: LMX2582 Hello E2E Team,
I am using ADC ADC12DJ3200 in my module.
I am giving 3.2GHz Clock signal through LMX2582 RFPLL as same as EVM.
I am getting NSD of -150.8 dBFs/Hz instead of datasheet value…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: , LMH6401 We use ADC12DJ3200 to work in JMODE2 mode. The received short transmission test mode data is normal, but when the ADC12DJ3200 normal sampling voltage value is set, the sampling voltage…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: TSW14J57EVM , Hi team,
One of our customer's issues, I'm forwarding it below, could you please provide some troubleshooting suggestions
When this customer is debugging the ADC12DJ3200 chip…
Hi Vaibhav,
Please find configuration and instructions attached. I have tested this by modifying our EVM to accept an external OSC input which I have supplied a 100MHz tone.
DAC39J84EVM_OSC_100MHz_1500MSPS_LMFS4421.pptx
DAC39J84EVM_100MHz_OSC_input_4421_1500MSPS…
Part Number: ADC12DJ3200
Can you please confirm the clock rate settings for 6 Gsps sampling rate for the ADC?
My understanding is that in single channel mode, the F_s * 2, so the device clock would need to be at 3 GHz. Is this correct?
Would a 300 MHz…
Part Number: ADC12DJ3200 Hi Team
I lsaw that the datasheet specifies the VOHmin which is 1.65v. What is the maximum output voltage?
Can i connect it directly to Xilinx FPGA 1.8V bank or do i need voltage translator?
Regards,
Roey
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: LMK04828 , LMX2485Q-Q1 Hello,
I have an application where I need a clock synthesizer to generate two clock signals (2.7GHz and 200MHz) from a 100MHz clock reference.
In the past, I remember seeing…