Part Number: ADC12DJ3200 Other Parts Discussed in Thread: TPS7A92 Hi team,
Due to stringent requirements for noise performance, one of our customers needs to use 2 LDOs to power digital voltage VD11 and analog voltage VA11, rather than use common 1.1VDC…
Part Number: ADC12DJ3200EVM Other Parts Discussed in Thread: LMK04828 Hi team
I am using internal ramp pattern to check whether it is properly been received at the FPGA side. I am using JMODE 2, with Fs=1250 MSPS. The Serdes is operated at 5Gbps.
As per…
Part Number: ADC12DJ3200 Hi @ all,
I'm currently a bit confused about the JESD line rate, specifically the way of calculation, could you please clarify.
My understanding, so far:
Linerate = Fclk x R
by Using JMODE 0, clk 800MHz
Linerate = 800MHz x 4…
Part Number: ADC12DJ3200 Hi team,
The customer uses jmode13 with 15bit effective bits. After 32-bit data is received, it is disassembled into I and Q channels with 15bit each:
The swing measured at the single end of AD input is 262mv, and the difference…
Part Number: ADC12DJ3200 I am unable to locate timing information for the OVR (out of range) signal for the the ADC12DJ3200.
i want to use OVR signal as a quick response signal to control another system.
So I need to konw the delay from the time when analog…
Part Number: ADC12DJ3200EVM The ADC12DJEVM is attached to a Xilinx XCVU13P using the JESDC core 4.2 from Xilinx. I am getting the link up correctly, but the upper 4 lanes are not receiving the ramp pattern that I see on the lower 4 lanes; or more specifically…
Part Number: ADC12DJ3200EVM Other Parts Discussed in Thread: ADC12DJ3200 , We are in the process to use ADC12DJ3200 chip in our design.
Could you share ADC12DJ3200EVM reference schematic?
Thanks,
Jimmy
Hello Kuwahara-San,
The ADC12DJ5200RF and ADC12DJ3200 are pin to pin compatible, for the schematic the ADC12DJ3200 symbol was just re used and this is a typo. The schematic is correct.
Best,
Eric
Part Number: ADC12DJ3200 Hi team,
One of our customers uses 2 pieces of ADC12DJ3200 and uses the mixer inside to complete the DDC operation. When trying to synchronize the NCO of two ADCs, it cannot be completed.
The customer tried to synchronize using…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: ADC08DJ3200 Hi team,
When selected JMODE0, output data consists of 12-bit data, the ENOB is about 8 bits;
When selecting JMODE4, output data consists of 8-bit data. What is its ENOB? This parameter…