Part Number: ADC12DL3200 I have a design using a single ADC12DL3200 device and capturing the ADC data inside an FPGA using the 4 LVDS buses from the ADC chip. I don't have the SYSREF signal connected to the ADC chip, and I'm finding that the ADC samples…
Part Number: ADS5409 Other Parts Discussed in Thread: ADS5402EVM , , ADC12DL3200 , LMK04832 , LMK04828 , LMK61E08 Tool/software: Hi Team,
1) In the below image of ADS5402EVM, Pin number P10, N10 are used as trigger pin function. But in datasheet it mentioned…
Part Number: ADC12DL2500EVM Other Parts Discussed in Thread: ADC12DL3200 Tool/software: Is a schematic available for the ADC12DL2500EVM / ADC12DL1500EVM / ADC12DL500EVM?
I cannot find one on any of these evaluation board webpages.
Design files would ideal…
Part Number: ADC12DL3200 Other Parts Discussed in Thread: LMX2594 Dear Sirs,
I've designed a board where a T&H samples a RF signal and then the T&H output signal is sampled by an ADC12DL3200.
The T&H has a 4 GHz clock signal and the ADC12DL3200…
Part Number: ADC12DL3200 Hi, there :
The signal we are interested is a signal with bias voltage (0.9V), but the input common-mode voltage of ADC12DL3200 is 0V.
The signal BW ranges from DC to several hundred MHz, so we can only use DC couple interface…
Part Number: ADC12DL3200 Hello E2E,
I have some questions about the power sequence of ADC12DL3200 on page 131 in datasheet.
The power sequencing requirement is VA19 ≥ Vx11.
What is the impact if we don't follow the rule?
May it damage the device…
Part Number: ADC12DL3200 Hello,
I am using the above mentioned @ 800Mhz sampling rate and trying to capture the data in FPGA and I am having trouble capturing the fixed data pattern. Can someone please provide reference design for the register values…
Part Number: ADC12DL3200 Other Parts Discussed in Thread: ADC12D1000 , ADC12D1600 Hello E2E,
Our customer is studying ADC12DL3200.
They would like to know the ripple requirement on VA19, VA11, VD11, and VLVDS, respectively.
In terms of ADC performance,…
Part Number: ADC12DL3200 I've seen the reference design source code in the forum. Is the reference design for ADC12DL3200 reference design code xilinx available in another location? Box doesn't allow me to access the file.
Thank you,
Zeki
Part Number: ADC12DL3200 Hello E2E,
I'm studying ADC12DL3200.
I want to know what are the three Electrical Characteristics as follow in datasheet Page 18, 22.
Are there all no input? How to analyze them? Thank you!