Part Number: ADC12J1600EVM Tool/software: WEBENCH® Design Tools Hello,
I'm, working on some device in automotive and I would like to use your product "ADC12J1600EVM - ADC12J1600 12-Bit, 1.6-GSPS, RF Sampling Analog-to-Digital Converter Evaluation Module…
Part Number: ADC12J1600EVM Hello,
I am using the ADC12J1600EVM together with the TSW14J56EVM.
In my application I need to operate the ADC12J1600 at its minimum voltage range of 500mV. I have changed that parameter in the GUI under the window Control/Gain…
Part Number: ADC12J1600EVM Hi,
I want to use the pin headers on the board to connect an FPGA board and program the devices externally using SPI over the connectors
instead of using the FTDI chip apart from connecting some wires , do i need to mod the…
Part Number: ADC12J1600EVM Hello,
I am trying to setup the ADC12J1600 evm in the default mode to see its performance. The ADC GUI says it can't detect an FTDI device(img 1). In spite of power cycling the EVM and unplugging/plugging back the USB, the error…
Part Number: TIDA-01573 Other Parts Discussed in Thread: OPA857 , OPA857EVM-978 , ADC12J1600 , LMG1020 , LMG1020EVM-006 Tool/software: WEBENCH® Design Tools Hello, I'm, working on some device in automotive and I would like to use your products (TIDA-01573…
Part Number: ADC12J1600EVM Hello,
I am starting to use the ADC12J1600 together with the TSW14J56.
Following the specification file slau56.pdf. I installed both the ADC12J1600EVM GUI and the High Speed Data Converter Software. The TSW14J56 connects properly…
Part Number: ADC12J1600EVM I'm currently working with ADC12J1600EVM (LOT: 3402150WBG) which I believe is version A. It has a TRF3765 VCO on board. However, the ADC12J1600EVM gui version v1.3.1 that I was able to download comprises the LMX2581.
Is…
Part Number: ADC12J1600EVMADC12J1600EVM: FTDI Device Error at GUI start up
Hello support team,
My customer has a problem on the ADC12J1600 EVM at GUI start up. Error message is "FTDI Device not connected properly !!!"
They have installed the…