Part Number: ADC12J4000 Other Parts Discussed in Thread: ADC12DJ3200 Hello again!
During last experiments with adc12j4000, we encountered unexpected behavior of device.
ADC produces significant spur at Fs/4. It happens in different modes (bypass, dec…
Part Number: ADC12J4000 Hi,
Customer is using ADC12J4000EVM, then I have a question about ADC Test Pattern. The ADC sent the ADC Test Pattern, however, the FPGA received the different data as follows. Please let me know the root cause of this issue.
…
Part Number: ADC12J4000 Other Parts Discussed in Thread: DAC37J82 Hello,
I have a component which generates SYSREF pulses for my ADC12J4000 & DAC37J82IAAV .
As I say in the title, this component generates a pulse on the LVDS differential inputs but…
Part Number: ADC12J4000 Other Parts Discussed in Thread: LMX2594 , , ADC12DJ3200 Hi,
I am trying to link ADC12J4000 to xilinx xc7vx690t by xilinx jesd204b ip core on my board, we are using lmx2594 so the sampling clock could up to 4GHz, we are going to…
Part Number: ADC12J4000 What is the definition of the differential full scale input range for the ADC12J4000? The data sheet shows that the full scale range can be set between 500mV and 950mVpp (7.3.5.4), it is not clear if this is 500-950mVpp after a…
Part Number: ADC12J4000 Other Parts Discussed in Thread: TRF3765 , Hi,
I'm confirming serial link parameters of ADC12J4000.
(1)For bypass mode, what is the difference Table 12 and Table 13 in the datasheet?
(2)How do I determine K factor? K has 4 to…
Part Number: ADC12J4000 Hi,
I'm using the ADC12J4000 EVM with the provided demo GUI and a FPGA Arria10 board, everything is working well : i can get adc i/q with no problem.
However when I move to my custom hw design, some problems with JESD start…
Part Number: ADC12J4000 Other Parts Discussed in Thread: LMK04828 ,
Hello!
I have board with FPGA Kintex UltraScale, LMK04828 and ADC12J4000 running at 3 GHz in bypass mode (6Gbps line rate). LMK provides 3 GHz clock to ADC, single 150 MHz clock to Kintex…
Part Number: ADC12J4000 Hi,
We want 6 Gsps ADC for our application, and the there is no specific ADC module which meets this requirement also. So, we want to use two interleaved 4 Gsps ADCs (ADC12J4000). We will 180 degrees phase shifted clocks for theese…
Part Number: ADC12J4000 We are evaluating the ADC12J4000 ADC using both the ADC12J4000EVM and the TSW14J56EVM . The TSW14J56EVM is running with its original firmware. Spectral display (FFT) looks fine when injecting RF carrier signal. However, result looks…