Part Number: ADC12QJ1600 Tool/software: Hello,
What is the difference time delay ( if exist ) between P and N of the high speed serialized outputs?
Regards,
Giora
Part Number: ADC12QJ1600EVM Other Parts Discussed in Thread: ADC12QJ1600 , Tool/software: Hi all,
ADC12QJ1600 is stated to have 6GHz 3db bandwidth. The supplied S-parameters starts at 50MHz. Can this ADC also sample 10MHz sinewave signal? Or go downto…
Part Number: ADC12QJ1600 Tool/software: hello,
When working with JMODE 8( 64/66b) does the chosen four outputs maps as:
Lane 0 to D0(+,-) , Lane 1 to D1(+,-),Lane 2 to D2(+,-) and Lane 3 to D3(+,-)?
Regards,
Giora
Part Number: ADC12QJ1600 Hello,
We are using JMODE8 664/66b and intend to use JCTRL.sync_sel =2 (do not use any sync input pin) use JSYNC_N as software sync.
Can we tie pin SYNCSE to GND permanently.
Giora
Part Number: ADC12QJ1600 Tool/software: Hello,
I would like to configure Microchip's JESD204B core for PolarFire FPGA together with the ADC12QJ1600 ADC.
Hardware has all 8 lanes connected to the FPGA.
I would like to use JMODE9 (8-bit, 8B/10B encoding…
Part Number: ADC12QJ1600 hello,
Do you have a release date for TI -JESD-204 -IP?
Where I can download it?
See the question and answer 3 months ago:
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1316519/ti-jesd204…
Part Number: ADC12QJ1600 Other Parts Discussed in Thread: LMH32401 Hello,
I design a new Lidar using the TIA LMH32401 connected to the ADC12QJ1600. (see schematic).
My question is : do I need to add input protection to the ADC inputs and if yes, do you…
Part Number: ADC12QJ1600-Q1 Hello,
I intend to design a board with X8 ADCQJ1600 devices connected to an FPGA - each ADC is connected to an FPGA through four
differential lanes ( 12 bit 64/66b JMODE 8 ). The ADC sampling rate is 1 GHZ.
My questions are…