Part Number: ADC14155QML-SP Other Parts Discussed in Thread: ADC14155 , We are considering the ADC14155 for our design but have some need of further data regarding it’s INL specification. Is there any more data regarding the INL and the sampling frequency…
Other Parts Discussed in Thread: ADC14155 Hi all: I am using the ADC14155LFEB/NOPB in conjunction with the WAVEVSN BRD 5.1/NOPB interfacing card. I want to do some RF testing with this set up, but I first need to know what the maximum input power of the ADC…
Other Parts Discussed in Thread: ADC14155 , CDCM7005-SP Hi
My clock is 128 MHz at 4.8 dBm, 50 ohm source. On the app note it shows a high speed buffer with a 24.9 ohm resistor in series to the ADC14155. Can I apply the clk directly (ac coupled of course…
5076.ADC14155 power.doc
Follow the link to power consumption vs. sample rate down to 35 MHz for a typical part. Assuming that it continues to be a linear curve, the power consumption at 20 MHz can be extrapolated to 740 mW.
Hello
I'm currently reviewing a design with a clock source of 128MHz to the ADC14155W-MLS. On the datasheet the maximum clock frequency is stated as 155 MHZ, but in the stress analysis it is currently failing the EEE-INST-002 frequency derating of 80…