Part Number: LMP91000EVM Other Parts Discussed in Thread: LMP91000 , ADC161S626 Tool/software: I'm trying to build heavy metal content on liquid with 3 leads electrode that the final result will be Cyclic Voltammetry and the concentration of the heavy…
Part Number: TMS320F280039C Other Parts Discussed in Thread: ADC161S626 Hi Team,
Here's an issue from the customer may need your help:
The F280039C SPI communicates with the ADC161S626. ADC16S262 needs 18 clocks to complete a data conversion. But…
Part Number: ADC161S626
Hi team,
If the ADC161S626 is been driven by a singe-ended source as below shown, and when Vref=2.5V,Vcm =2.5V, would the output of ADC161S626 be distorted?
Thank you!
Regards…
Part Number: ADC161S626 Hi,
I have a circuit like below:
The input range is 1 to 3V, I intended to use single-ended. Since I have only a positive signal, I connected the -IN pin to GND.
But when I tested I found that I have to do " 4 * " to get…
Part Number: ADC161S626
Hi expert,
My customer is using ADC161S626.
They give the IN- and IN+ almost the same voltage 2.5V, So the output should be about 0V.
and they try a twice 16bit read and a three times 8bit read to read the data.
however…
Part Number: ADC161S626 Other Parts Discussed in Thread: ADS8325 , TINA-TI Hi Experts,
Seeking your assistance on this query:
I'm a TINA-TI customer user, version n 9.3.200.277 SF-TI and I was studying some model simulations. Looking for the best…
Part Number: ADC161S626 Other Parts Discussed in Thread: TINA-TI , Hello E2E,
I downloaded the "snam.TSC" file from TI's web, and I tried to run it at transient analysis. However, it could not run with TINA-TI. www.tij.co.jp/.../snam110
I want to…
Hello Jens,
The ADC161S626 uses the SCLK for the conversion clock. This places a maximum SCLK period limit due to leakage currents inside the device, which is specified in the datasheet as a minimum SCLK frequency of 1MHz, or 1uS max period.
A conservative…
Fan,
I ran a transient analysis and got the plotted results shown in the image below. The circuit is attached here as well. Regards, John
6318.ADC161S626.TSC
Part Number: ADC161S626 Hello,
I am trying to send out the ADC value to my microcontroller(hercules) on SPI. The adc needs 18 clocks to push 16 bit data out but hercules has max word length of 16 bits. So I am doing 2 successive receives so that I get…