Hi, I am using the following part in my design . Can you please provide the Input Impedance details of following ADC as per the requested table below.
Part #
Frequency (MHz)
S11 Parameter
Zinput
ADC16DV160CILQ/NOPB
30
…
Part Number: TSW1405EVM Hello TI Community,
I am a digital hardware engineer. I want to make sure I am selecting the correct capture hardware for my ADC.
I would like to capture both channels of an ADC16DV160 to verify that I properly receive a…
I have faced same distorsion problem in my design with ADC16DV160. From two channel one channel is pretty clean, where as other channel was distorted. Initialy the distorsion was more. I found that it was DDR data Alignement problem with clock. I tried…
Characterization included performance measurements at 3.0V and 3.7V. Average SNR and SFDR was mostly flat betweeen the points, though the SFDR distribution spread. 197MHz -1dBFS input.
Regards, Josh
Hi Josh,
We are planning to use ADC16DV160 ADC input as 50Ohm for the full-scale of 2.0Vp-p configuration which is corresponds to +10dBm RF input power.
NSD = FScale - SNR - 10*log10(Fs/2) = +10 - 78 - 10log10(160e6/2) = --147.0 dBm/Hz
The NF at…
Josh,
sorry for the late reply, I've been on vacation.
Thank you so much for your thoughtful and very helpful answer again. You saved us a lot of wasted time.
Best Regards, Florian
Other Parts Discussed in Thread: ADC16DV160 Hello,
we want to compare the performance of ADC16DV160 vs AD9653. Where can we get the following datas for ADC16DV160?
1.) SNR for fin@9.7MHz?
2.) Power(per channel) @ 25Msps?
Other Parts Discussed in Thread: ADC16DV160HFEB Dear TI experts.
My customer want to use ADC16DV160 for new project which is a laser measurement system.
I found the FPGA image file (wave vision 5). However I wanna see the FPGA code for reference.…
Other Parts Discussed in Thread: ADC16DV160 Hi
I will request data about SFDR of ADC16DV160. Is there a characteristic graph of temp vs SFDR? (" Horizontal axis temp" - " vertical axis SFDR") For example , fin = 30M, fCLK = 160MSPS, VDR = 1.8V , -40…
Dear All,
Let me ask a question about ADC16DV160CILQ.
Please refer to attached file.
①In this case , how much is a phase difference between CLK+/CLK- and OUTCLK+/OUTCLK-?
②When a user performs phase adjustment of OUTCLK+/- (31°~143°),
does phase…