Part Number: ADC31JB68 Hi,
I was wondering if it is possible to get drivers for 24-bit SPI implementation in Linux for ADC31JB68. We are running Linux on Xilinx Zynq UltraScale+ SoC. The available drivers are meant for 8, 16, or 32-bit mode but the ADC…
Part Number: ADS5407 Other Parts Discussed in Thread: ADS54J64 , ADC12QJ1600 , ADC16DX370 , ADS4449 , ADC31JB68 Hello,
Please, read the previous questions and answers related to the ADS5407.
So, we plan a 4,000-Channel, 14-BIT, 500MHz ADC system with simultaneous…
Part Number: ADC31JB68 Other Parts Discussed in Thread: LMK04828 , Hi,
I am doing almost same test with ZCU106 board + TSW14J10(rev C) + ADC31JB68EVM(rev B).
I am using Agilent N5181A signal generator's 500MHz +12dBm output for CLK input.
I had reworked…
Part Number: ADC31JB68 Hello,
I am testing the ADC31JB68EVM with Xilinx ZCU102 board (FMC HPC1).
But I can read only serial S0 data from the JESD204 IP core output data, S1 looks random data pattern.
Also, I found readout data look jumps. I've attached…
Part Number: ADC31JB68 Hi,
We developed and FMC card based on ADC31JB68 ADC. I have the following setup my ADC input freq is 5 MHz but I only see 25 samples which means the ADC is sampling at 125 MHz. I need 4 times the samples with 500 MHz sampling freq…
Part Number: ADC31JB68 Hi Team,
My customer is looking for the land Pattern and size of the exposed thermal pad for ADC31JB68RTAT. These information is not included in the datasheet.
Regards, _Renan
Part Number: ADC31JB68 Hi!
Datasheet for ADC31JB68 allows to use one regulator for +1.2V nets with ferrite bead isolation of VACLK from other VA1.2 pins. Looking into EVM schematics, there is another filtered path - for pin 29. This pin (one of four VA1…
Part Number: ADC31JB68 As per the datasheet of the device , The device is meant for high IF sampling receivers and plots are provided according to that. I want to use the device for 1100 MHz using 500 MSPS sampling rate. Is there any reading in this frequency…
Hi Andrew
The ADC31JB68 performs periodic alignment character insertion to be in compliance with the JESD204B spec. In your case scrambling is disabled, so the rules for Character Replacement Without Scrambling will be followed. Here is an excerpt from…