Other Parts Discussed in Thread: ADC3222 Hi,
Let me ask you some simple questions about ADC3222 as below. (datasheet page 8)
1) Eg(REF)
This Gain error spec includes "internal reference error", correct?
2) Eg(CHAN)
And this Gain error spec…
Other Parts Discussed in Thread: ADC3222 Hi,
I will ask on Dither Disable Register (ADC3222).
Q1) It is written with the "Register 434h" in the data sheet (SBAS672A) page53 Table8 [3-2 DIS DITH CHB], but you thought that "Register 534h" is correct…
Other Parts Discussed in Thread: ADC3222 Hi
Let me three questions ADC3222.
Q1) How to print the CUSTOM PATTERN in CHA or will correct in the following order ?
1. address 0Eh = bit[7:0] is set to CUSTOM PATTERN
2. address 0Fh = bit[7:4] is set to CUSTOM…
Other Parts Discussed in Thread: ADC3222 Hi,
ADC3222 Unused pin
Please tell me the recommended circuit of free terminal processing.
1) Do not use the SYSREF function.
You set to "1" in the Bit0 of setting register 70Ah, do you want to how the treatment…
Other Parts Discussed in Thread: ADC3222 , ADS5281 , THS4521 , THS4541 Hi,
ADC3222 Front-end Circuit(Opeamp)
1) Although analog input is ± 1V = 2Vpp, does it can be used in single-ended.
If possible, please tell me the circuit configuration.
2)…
Hi Renan,
The ADC3222 family is actually not able to reliably sample under 15 MSPS (please see page 47 of the datasheet). Please feel free to send me an email if you would like to discuss further.
Best Regards,
Dan
Part Number: ADS4222 Other Parts Discussed in Thread: ADC12DL040 , ADC3222 Hi All
My customer is searching high speed A/D Converter that is compatible following specs.
(1) Dual and Simultaneous Sampling (2) Resolution : over 12bit (3) Sampling Rate : over…