Part Number: ADC3224
Hi TI team,
We manufactured 20 ADC boards using the ADC3224 chip. Among them, ten boards exhibit approximately 30 bits of noise fluctuation on the FPGA data output when the ADC input voltage is zero(connect to VCM thru. 0.1uF…
Part Number: ADC3224EVM Other Parts Discussed in Thread: THS4541 , ADC3224
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
Sometime ago, I have ordered ADC3224EVM from TI to make some demo applications for Analog…
Part Number: ADC3224
Hi Team,
I have a question about ADC3224 Initialization.
Datasheet mentions below.
Dose this mean after applying a high pulse on the RESET pin, ADC3224 automatically initialize internal registers to default values or do…
Part Number: ADC3224 Hello,
SYSREF function and usage is not explained in datasheet.
So when and how I supposed to use it?
Who aperture delay varies over temperature +20..+50C. And how delay variation over temperature between parts behave?
I expect…
Part Number: ADC3221 Other Parts Discussed in Thread: ADC3224 , Customer needs IBIS model of ADC3221. IBIS model of ADC3224 is on ADC3221 web page.
IBIS model of ADC3221 is same as ADC3224's?
Part Number: ADS62C15 Other Parts Discussed in Thread: DAC5672 , , ADC3422 , ADC3224 , ADC3644
Tool/software:
Hi TI supporter, I am looking for the ADC 125 Msps include 2 channel /chip with parallel interface (at least 12 bits). And the DAC up to…
Other Parts Discussed in Thread: ADS4145 , ADC3244 , ADC3224 , ADC3664 The infrared signal containing noise is divided into two signals so that the phase is 180 degrees. Communication data is communicated at 1 mhz, and at this time, it converts even ambient…
Hi Mano,
Yes, most of our ADCs are suited for AC and DC coupling applications. Yes, wider input bandwidth does support higher IF applications like SDR, but can also be used for applications that don't required high input bandwidth.
What sampling frequency…
Art:
The DAC samples up to 250 MSPS. 1st Nyquist zone is up to 125 MSPS. It would be tricky to transmit at 156-162 MHz within the second Nyquist zone, but possible with a reduction in output power due to SINC roll-off.
The ADC samples up to 125 MSPS…
Bagher:
Check out the ADC3224 12-bit, 125 MSPS device. This is a dual but is low cost and low power. You can disable one of the channels if desired. This one should work nicely in your application.
--RJH