Part Number: ADC3244 Hello,
On page 48, in section 9.31 the data sheet for the ADC3244 (and other ADCs) says,
"9.3.1 Analog Inputs
The ADC324x analog signal inputs are designed to be driven differentially. Each input pin (INP, INM) must swing symmetrically…
Part Number: ADC3244 Hi
The datasheet (SBAS671B) page 48 section 9.3.2 states "the device clock inputs can be driven differentially or single-ended, with little or no difference in performance between them." The following page states "However, for best…
Other Parts Discussed in Thread: ADC3244EVM , ADC3244 I have connected an ADC3244EVM board via mini USB to a PC running the ADC3000 GUI. On start up, the GUI correctly reports 0x00 for all registers. Any subsequent reads, however, report 0xFF. I have seen…
Other Parts Discussed in Thread: ADC3244 I am interesting in "ADC3244" and reading it's datasheet. There is a information which I do not get it in datasheet. The default setting of digital data output is one wire or two wire.
Hi Shyam, another option is to directly sample the 200MHz input, however resolving an 8kHz tone may be challenging. If you think about this route, a few of the ADC suggestions we have at these speeds would be ADC3244 or ADC3664. If you decide to go the…
Hi Eunjae,
Please check out the ADC3664, ADC3244, ADC3224. These might be a good fit from what I understand in your block diagram.
If you have other requirements please feel free to ask another question.
Regards,
Rob
Part Number: ADC3244EVM Other Parts Discussed in Thread: ADC3244 , Hi team,
Please help the customer with issue bellow.
there is not a clock oscillator available on this board. I have to connect a 125MHz clock to this board from an external clock source…
Hi Xiaoqiang,
Since the ADC3244 has an unbuffered analog input, the low pass filter cutoff frequency (fc) should be at or below the sample rate. Doing this will help to attenuate the glitch/kickback energy from the switching of the ADC sample/hold capacitors…