Nhi,
We can offer the following LVDS devices:
Speed (Msps) bits Part # # of Converters
125 12 ADS4125 1
125 14 ADS4145 1
80 12 ADC3223 2
80 14 ADC3243 2
125 12 ADC3224 2
125 14 ADC3244 2
If you prefer JESD204B parts we can recommend these as well.
Regards,
Ji…
Part Number: ADC32J44 Other Parts Discussed in Thread: ADC3244 , Please can I have more details on the flicker noise performance of the ADC32J4x range. My application requires 'full ADC performance' measurements (ie ~-150dBFS/Hz) down to offsets as low…
Part Number: ADC3244EVM I'm using ADC3244 EVM, running it by default settings (two-wire mode). Given 60MHz CLKIN, I got 30MHz FCLK and 210MHz DCLK. The analog input channel is driven by constant voltage.
According to the datasheet, the ADC samples…
Gordon,
The TI EVM actually has an option to use an amplifier as an input source. See the attached schematic. This is an example you can use.
There is a little bit of 1/f noise close to DC on this ADC you will need to take into account. There is an LVDS…
Hi Richard,
Thanks for the detailed reply. I understand the EVMs are designed for the most common AC coupled applications your customers use these high speed ADCs for. Our application is for acquiring near DC signals from a sensor array. We are switching…
Other Parts Discussed in Thread: ADC3244 Hello,
After some forum help I am able to read and parse the HSDC software output binary data file. I'm using the TSW1400EVM and the ADC3244EVM. The ADC3244EVM has a 14 bit ADC3244 converter on it. The ADC is…
Other Parts Discussed in Thread: ADC3244 Hello,
I'm using the HSDC Pro software and I have to pass the ouput/acquired time domain data to other software for processing. So, I'm looking through the HSDC Pro Software documentation and I'm not seeing…
Other Parts Discussed in Thread: ADC3244 , LMH6553 The ADC3244 has a 2.1V max input at the ADC. My signal from the output of the previous stage is single ended. The voltage could go as high as 5V and while this is not a problem from the point of view of…