Part Number: ADC3244EVM We are using TSW1400EVM and ADC3244EVM.
A warning will appear if the Firmware is not found.
GUI is displaying Firmware Version 15.15
We installed the GUI.
.rbf is not found in the specified folder.
We want the rbf file…
Part Number: ADC3244EVM Hi,
We currently use 2 ADC3244 ADCs in a dual receiver architecture. We are experiencing an issue with receiver B not working during startup due to synchronization issues. Our start-up sequence is to rest all ADCs, set up each…
Part Number: ADC3244EVM Hello,
I was wondering what the purpose of the four transformers on page two of the ADC3244EVM's schematic (see below) were? Is it an isolation transformer or something else? And are they necessary for operation?
0410.ADC32XXEVM…
Part Number: ADC3244EVM Hi team,
Please help the customer with issue bellow.
I want to use THS4541 differential amplifier onto the board to amplify my input signal by the gain 10 V/V. To do this, I will first modify the board to arrange it in DC-coupling…
Part Number: ADC3244EVM Hi team,
Please help the customer with issue bellow.
there is not a clock oscillator available on this board. I have to connect a 125MHz clock to this board from an external clock source. My question is, what should be the…
Part Number: ADC3244EVM I recently got hold of an ADC3244EVM and was looking to pair it with a TWS1400EVM in order to capture data for a project. On the TI website it is advertised as a dual channel Dev board but upon receiving it I noticed that there…
Hi Yahwen,
Were you able to find a solution this issue? Due to thread inactivity, I will go ahead and close this thread. If you require further assistance, please create a new post.
Best Regards,
Dan
Jim,
I'm using the ADC3244EVM. I don't think it has multiple operating "modes". I'm sampling a single channel anywhere from 65 MSPS to 125 MSPS.
Thanks.
Roger