No, Ken, the status lights do not change in any way. The board that I'm using with the TSW1400 is the ADC3244EVM.
Here (below) are photos of the board(s)..
Hi Roger
I'm glad you're able to read and parse the binary data file.
The reason the numbers appear to be in offset binary instead of 2's complement is because of some processing done in the High Speed Data Converter Pro software.
Each ADC used…
Other Parts Discussed in Thread: ADC3244 I have connected an ADC3244EVM board via mini USB to a PC running the ADC3000 GUI. On start up, the GUI correctly reports 0x00 for all registers. Any subsequent reads, however, report 0xFF. I have seen this problem…
Hi Richard,
Thanks for the detailed reply. I understand the EVMs are designed for the most common AC coupled applications your customers use these high speed ADCs for. Our application is for acquiring near DC signals from a sensor array. We are switching…
Hi Zhonghui,
1. The maximum sampling rate of ADC3244E is 125msps, and the estimated total transmission rate should be 2gbps. It supports serial LVDS interface, but it is found that the upper limit of serial LVDS interface rate is 1.0gbps, which is less…
Part Number: ADC3224EVM Other Parts Discussed in Thread: THS4541 , ADC3224
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
Sometime ago, I have ordered ADC3224EVM from TI to make some demo applications for Analog…
slau579d.pdf Leejh,
Connect a 80Msps clock (or lower) to SMA J9 with a power of at least 10dBm. See section 1.4 and figure 7 of the attached ADC3423EVM User's Guide.
Regards,
Jim