Part Number: ADC34J45 Other Parts Discussed in Thread: LMK04828 , ADC32J45 , , DAC37J84 , ADC34J24 HI,
To change the ADC / DAC from serial LVDS to JESD204B, our customers are considering a signal chain by combining the following products.
/ LMK04828 / ADC32J45…
Part Number: ADS54J42 Other Parts Discussed in Thread: ADC32J45 , DEARS.
The customer designs the ADC32J45 and ADS54J42.
The ADC32J45 has design experience.
But the ADS54J42 is first designed.
Please review the ADS54J42 related circuit.
There was a SNR…
Hi Jim B
The setting values of the following files are the same.
The Register values of 80Msps, 128Msps and 160Msps are the same.
All values are zero.
ADC3xJxx_80MSPS_Operation_LMK_Setting.cfg
ADC3xJxx_128MSPS_Operation_LMK_Setting.cfg
ADC3xJxx_160MSPS_Operation_LMK_Setting…
Torsten,
Just an FYI, all of our JESD204B ADC EVMs use the same connector so the connector on the ADC32J45 and ADC32RF45 have the same samtec connector. Although Richard refers to the ADC32RF45, this is the same connector on the ADC32J45EVM.
Ken.
Hi Kaede,
Could you please confirm whether the Vin for the THS4541 is open or connected to 1.85V? It is a bit confusing from your post to determine exactly what it is.
Also, could you please provide the actual schematic which is used for interfacing…
Andrea,
You can certainly use a transformer to convert the differential output to single-ended, however you will lose any dc effect because of the transformer. As long as the bandwidth of the transformer meets your requirements you should be okay.
In…
Good idea RJH. thanks
here is a direct link to the newer mutli-channel ADCs with lower power
4-ch 14-bit with JESD204B outputs http://www.ti.com/product/adc34j45
4-ch 14-bit with serial LVDS outputs http://www.ti.com/product/adc3444
Also look for the 2…
Part Number: IPNC-RDK-CSK Tool/software: TI C/C++ Compiler I installed IPNC_RDK_3.9.1.tar.gz and I want want to compile source but (make sysall) following the ( processors.wiki.ti.com/.../IPNC_RDK_DM38x_,_DM8127) but after successful compilation but there…
Hi All,
I want to design a WiFi operated Smart LED Bulb with Standard AC input and Also need to control dimming via micro controller as well as will drive WiFi module also.
Can anyone suggest me any solution for these requirement.
Can you suggest me IC…