Other Parts Discussed in Thread: LMK04828BEVM , ADC32RF80EVM , LMK04828 , ADC32RF45EVM , LMX2592 , ADC32RF80 I connect the CLKin* of LMK04828BEVM to signal generator and set the frequency to 122.88MHz and connect the DCLKout0 and DCLKout10 to J7 and J5 of ADC32RF80EVM…
Other Parts Discussed in Thread: ADC32RF80EVM , TSW14J57EVM , ADC12DJ3200EVM , LMK04828BEVM Hi TI Engineer:
Question 1: Regarding ADC32RF80EVM board, the recommended data acquisition card in the description on TI official website is TSW14J56EVM. Can I use…
Part Number: ADC32RF80EVM
I have an ADC32RF80-EVM development board and I need to download the ADC32RFxx EVM GUI Installation software from the website. However, each time the software starts to download for a few minutes, it will display "Failed - need…
Hi Gavin,
It is best to use the ADC32RFxx GUI to generate the proper configuration. Please refer to the following software link and user's guide. The auto configuration wizard should help guide you through the configuration process
https://www.ti…
Dora,
The TSW14J56EVM from TI was not designed to work with AD products. This EVM will work with a TI ADC32RF80EVM, which may be an alternate solution for your application.
Regards,
Jim
Hi Maohang,
This is not an error. It is an expected pop-up to inform the lane rate and clock expected by TSW14J56. You can click OK and continue.
Also regarding the ADC capture issue, I setup this EVM on my bench and tested it. I see that after powering…
If we use ADC32RF80EVM and ADC12DJ3200EVM at the same time and want ADC32RF80EVM and ADC12DJ3200EVM to synchronize, do we need to use LMK04828BEVM for control? Or direct ADC32RF80EVM and ADC12DJ3200EVM interconnects to synchronize。
Hi,
ADC32RF80 doesn't support bypass modes. For bypass mode, you'll need ADC32RF4x device.
The device doesn't support 14-bit mode at 2949.12MHz due to SerDes rate limitation. The max rate is 12.5Gbps.
If you have ADC32RF80EVM, you'll have…