Part Number: ADC3423 Other Parts Discussed in Thread: ADC3424 , ADC3443 , Hi All,
I want to know INL and DNL of ADC3423/ADC3424/ADC3443, but I can't find it in the datasheet. Please give me some information about INL and DNL.
Best Regards, Ishiwa…
Part Number: TSW1400EVM hi
I bought the tsw1400 and adc3423 board and connected it like a picture
I ran it using HSDC (v5.0) software.
However, the test has failed because of the message like the picture.
The problem seems to be that USER_LED3…
Part Number: TSW1400EVM Tool/software: TI C/C++ Compiler hi guys~
can I use Labview with ADC3423 EVM?
does Ti support Labview library?
If supported, how can I download it?
Hello
I don't fully understand the role of the SYSREF signal in the ADC3423 .
Is it needed only for part to part synchronization? If i have only one ADC can I leave the SYSREF pins open?
Is there a way to synchronize multiple ADC's without sysref…
Other Parts Discussed in Thread: ADC3423 Hi Team,
We want to work with the ADC3423 at 80MSPS using two-wire LVDS at 480MSPS.
What should be the DCLK rate ? 80/120/480 ?
What should be the relationship between the DCLK and CLKIN ?
Best regards…
i felt very happy when i have seen models like ADC3423 , what i did not understand is how to see the dataoutput
for example the TINA reference design given for download on ADC3423 product page gives a design , which has input connected and IC being…
Part Number: ADC3423EVM I want to generate a test pattern from the ADC3423 on the EVM, which is connected to an fpga with a FMC-ADC .
I am using the ramp pattern. Except for the apparently known issue that the ramp only increases every 4th clock cycle…
Other Parts Discussed in Thread: ADC3423 , TINA-TI i felt very happy when i have seen models like ADC3423, what i did not understand is how to see the dataoutput
for example the TINA reference design given for download on ADC3423 product page gives…
Other Parts Discussed in Thread: ADC3423 Hello,
If I want to get an SFDR better than 60 dBc for the ADC3423, close to a zero IF signal, what is the max amplitude ripple allowed at the analog Vdd and digital Vdd ?
The PSRR is lower at the very low…
Other Parts Discussed in Thread: ADC3423 Hello,
In the register 15h, Bit 3, it is written "The ADCs of both channels enter standby":
Which pair of both channels AB or CD enter to the standby mode ?
During the standby power down, is the device…