Part Number: ADC3442EVM Hi Team, seeking for some clarification.
Is TSW1405EVM compatible wth ADC3442EVM? I think that the TSW1405EVM is compatible to read (short) waveforms from ADC3442EVM. But please confirm that for me too.
Thank you.
-Mark
Part Number: ADC3442EVM Other Parts Discussed in Thread: ADC3442 Dear Sir/Madame, I hope this message finds you well.
I am Dimitris Gounaridis, a researcher based in Athens, Greece, reaching out to explore the capabilities of your ADC systems for a…
Part Number: ADC3442EVM I am using adc3442evm .
When calculating the resolution, I want to know if I should use 5V or 1.8V to calculate it.
5V/(2^14) or
1.8V/(2^14)
Part Number: ADC3442EVM I want to get differential output with ADC3442EVM.
Signal input is possible through J1, J4, J5, and J8. However, it seems that the input does not go through J2, J3, J6, J7. When I want to give differential input, should I change…
Part Number: ADC3442EVM Other Parts Discussed in Thread: ADC3442 I am using ADC3442EVM.
The sampling rate used in the manual is 125 MHz.
By the way, when setting to HSDC, it seems that it is possible to set up to 160MHz.
Please tell me the maximum sampling…
Part Number: ADC3442EVM Other Parts Discussed in Thread: ADC3441 , ADC3444 , ADC3443 , ADC3442 In the case of the ADC3442EVM, I know that it has a specification of 50MSPS.
However, in the test setup of the manual, 125M is to be used.
In addition,…
Part Number: TSW1400EVM Other Parts Discussed in Thread: ADC3442EVM Previously I posted a question. However, it didn't solve the problem. https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1191313/tsw1400evm-time…
Part Number: ADC3442EVM Other Parts Discussed in Thread: ADC3442 Hello Team,
may I kindly ask you to provide the ADC3000 GUI to configure the ADC3442 on the EVM, please?
Thanks and Best Regards, Hans