Part Number: ADC34J45EVM Other Parts Discussed in Thread: ADC34J45 Tool/software: I'm using the TI software SW "ADC3000 GUI" Build date: 002/23/2022 to configure the ADC34J45. The possible setting in the software do not reflect the register…
The datasheet of the ADC34J45 does not describe such a register. Where do I find some info about his hidden register? Are there more such registers not being documented?
Part Number: LMK04828 Other Parts Discussed in Thread: ADC34J45 Hello,
We are working in a design where LMK04828 is connected to an ADC (ADC34J45) and we need to know which the configuration of LMK4828 outputs is (i.e. disabled or enabled) when LMK04828…
Part Number: ADC34J45 Dear All,
Hi.
I'm using ADC34J45EVM with TSW14J56EVM.
I have a question about converting the ADC code to the corresponding voltage value.
I read this blog post:
# e2e.ti.com/.../it-s-in-the-math-how-to-convert-adc-code-to-a-voltage…
Part Number: ADC34J45 Hi,
I read the doc " ADC34J4x Quad-Channel, 14-Bit, 50-MSPS to 160-MSPS, Analog-to-Digital Converter with a JESD204B Interface". I want to confirm:
1, After Power on, the ADC34J45 send the K28.5 if the SYNC is high. If…
Part Number: ADC34J45 Dear Technical Support Team,
I have a question about schematic of EVM.
Datasheet shows that 46pin and 39pin are AVDD.
However, the schematic of "ADC3XJXXEVM-SCH_B.pdf" says that 46pin is AVDD and 39pin is IOVDD.
These are…
Part Number: ADC34J45
Hi.
I'm using ADC34J45EVM with TSW14J56EVM.
I want to ask if it is necessary to ground the units in case they are connected to a source which is in the outdoors. I'm afraid that possible ESD or other things may have negative…
Part Number: ADC34J45 Hi.
I have a question regarding ADC raw time domain data.
I want to ask whether or not I can access ADC raw time domain data in LABVIEW.
Reading the user guide in HSDCPro Automation DLL\Manual and Examples folder, I found that there…
Part Number: ADC34J45
Hi,
The input signal to all four ADC is the same signal.
How can I test if data is align between all 4 ADC channels on my board?
Beset Regards,
Ran
Part Number: ADC34J45
Hi,
I'm trying to test the JESD204B SerDes of ADC34J45 using the test pattern feature.
I set register 0x06 with 0x02, and tried several option according to data sheet:
0x0A,0x0B
Datasheet
Measured
0x11
All 0's
OK …