Part Number: ADC3642EVM Other Parts Discussed in Thread: TSWDC155EVM Tool/software: Hi Rob,
Thanks for your suggestion.
I purchased the suggested part(TSWDC155EVM) to interface with ADC3642EVM.
I made the test setup and configured the ADC3642EVM…
Part Number: ADC3642EVM Other Parts Discussed in Thread: TSWDC155EVM , ADC3642 Tool/software: Hi,
I'm working on a project involving ADC3642EVM Evaluation module. In order to test the board we needed an FMC card which is TSW1400EVM. We found that it…
Part Number: ADC3642EVM Other Parts Discussed in Thread: ADC3643EVM Hi,
Yes you mentioned you would update the page to include a reference design? Can you please add a reference design for the ADC3642EVM.
Cheers
Part Number: ADC3642EVM Other Parts Discussed in Thread: ADC3643EVM , Hi Team, Can we request for the design files of the ADC3642EVM for our customer? Unlike the ADC3643EVM, it seems that it isn't available in its product page. Thanks in advance! Kind…
VOCM of THS4541 is connected to VCM of ADC3662. it is 0.95 V.
This is the same part as the EVM. ( ADC364xEVM_RevF(004)_Sch_2022-04-01.pdf )
When wired as is the current circuit, when 20 mA flows, the output saturates at 2.6 V. (except ADC3662, VOCM…
Hi Balvan,
Yes, this should be stable since the 100 ohm resistors are acting to isolate the capacitive loading of the ADC from the amplifier (too much capacitive loading on the amplifier output will cause oscillation. See this article - Why Op Amps…
Hi Pieter,
I see you've come across the collector's edition of the ADC3660EVM = )
In all seriousness, my apologies for the inconvenience/confusion. The schematic that reflects the board that you have in hand is attached.
6840.DC104C(001)_Sch.pdf…
HI Matti,
DC104C(001)_Sch.pdf DC104C(001)_Assy.pdf
Attached are the correct schematics and assembly file for the ADC3643EVM that you have. Apologies for the confusion.
Best Regards,
Dan